【i.mx.rt1061】 How does enet support hot plug function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

【i.mx.rt1061】 How does enet support hot plug function

ソリューションへジャンプ
2,791件の閲覧回数
bobhi009
Contributor I

Hi:

    SDK ver: 2.6.2 EVKB IMXRT1061

I use the usb、sai、and  enet. 

I hope that the USB and SAI interfaces can be used normally When I do not plug in the network cable。

But now if I don't plug in the network cable when I init the enet,  It will block all the task .

bobhi009_0-1631330809430.png

 

How does enet support hot plug function ?

0 件の賞賛
返信
1 解決策
2,776件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @bobhi009 ,

   I find your ethernetif_phy_init API already add the timeout count, do you test it, if you didn't plug the network cable, debug the code, whether it can go over through the while, then do the other module initializing? Or it still stay in the ethernetif_phy_init?

  In fact, just need to add the timeout, when the time is reached, and the network cable still didn't plugin, just go over that code, and don't do other enether coding.

  Please debug your code and test it again.

 

Best Regards,

Kerry

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,777件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @bobhi009 ,

   I find your ethernetif_phy_init API already add the timeout count, do you test it, if you didn't plug the network cable, debug the code, whether it can go over through the while, then do the other module initializing? Or it still stay in the ethernetif_phy_init?

  In fact, just need to add the timeout, when the time is reached, and the network cable still didn't plugin, just go over that code, and don't do other enether coding.

  Please debug your code and test it again.

 

Best Regards,

Kerry

0 件の賞賛
返信
2,772件の閲覧回数
bobhi009
Contributor I

Hi Zhou:

    I set the ENET_ATONEGOTIATION_TIMEOUT to '2' , and disable the assert , it can go over now .

 

0 件の賞賛
返信
2,770件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @bobhi009 ,

   Thanks for your updated information.

   Yes, you are right, you can change the timeout time, it is totally controlled by the customer requirement!

   If your issue is solved, please help to mark the correct answer, just to close this case, any new issues in the future, welcome to create the new question post.

Best Regards,

Kerry

0 件の賞賛
返信