Using DMA for SPI, how to configure SPI settings?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using DMA for SPI, how to configure SPI settings?

5,252 次查看
jackking
Senior Contributor I

Looking at the DMA example for SPI, it doesn't perform any SPI configuration other than selecting the SPI base.

How is the SPI peripheral configured?  Specifically frame size and chip select... 

In other posts, it looks like the block of DMA memory should be interspersed with command data before initiating the transfer, but I don't see this in the SDK example.

Any tips?

0 项奖励
回复
5 回复数

4,793 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jack King,

Please tell us which processor you used, thanks.

BR

Alice

0 项奖励
回复

4,793 次查看
jackking
Senior Contributor I

I am using the IMXRT1050.

0 项奖励
回复

4,793 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jack,

I guess you mean the CMSIS demo, in CMSIS, functions includes SPI Initialize, SPI send and others all

build in to cmsis lib.

I recommend you use SDK driver and demo:

pastedImage_1.png

we can find the configuration clearly :

pastedImage_2.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

4,793 次查看
jackking
Senior Contributor I

That code that you posted doesn't exist in the IMXRT SDK example for lpspi. 

SDK_Import_Wizard_and_workspace_-_evkbimxrt1050_cmsis_lpspi_edma_b2b_transfer_master_dma_spi_master_source_cmsis_lpspi_edma_b2b_transfer_master_c_-_MCUXpresso_IDE.jpg

It only has:

workspace_-_evkbimxrt1050_cmsis_lpspi_edma_b2b_transfer_master_dma_spi_master_source_cmsis_lpspi_edma_b2b_transfer_master_c_-_MCUXpresso_IDE.jpg

Which doesn't set PCS or frame size...

Here is the full example code:

/*
 * Copyright 2017 NXP
 * All rights reserved.
 * 
 * SPDX-License-Identifier: BSD-3-Clause
 */

#include "fsl_device_registers.h"
#include "fsl_debug_console.h"
#include "fsl_lpspi_cmsis.h"
#include "board.h"

#include "fsl_common.h"
#include "pin_mux.h"
#if ((defined FSL_FEATURE_SOC_INTMUX_COUNT) && (FSL_FEATURE_SOC_INTMUX_COUNT))
#include "fsl_intmux.h"
#endif
/*******************************************************************************
 * Definitions
 ******************************************************************************/
/* Master related */
#define DRIVER_MASTER_SPI Driver_SPI3
#define EXAMPLE_LPSPI_MASTER_IRQN (LPSPI3_IRQn)
#define EXAMPLE_LPSPI_DEALY_COUNT 0xfffffU
#define EXAMPLE_LPSPI_MASTER_DMA_MUX_BASEADDR DMAMUX
#define EXAMPLE_LPSPI_MASTER_DMA_BASEADDR DMA0

/* Select USB1 PLL PFD0 (720 MHz) as lpspi clock source */
#define EXAMPLE_LPSPI_CLOCK_SOURCE_SELECT (1U)
/* Clock divider for master lpspi clock source */
#define EXAMPLE_LPSPI_CLOCK_SOURCE_DIVIDER (7U)

#define EXAMPLE_LPSPI_CLOCK_FREQ (CLOCK_GetFreq(kCLOCK_Usb1PllPfd0Clk) / (EXAMPLE_LPSPI_CLOCK_SOURCE_DIVIDER + 1U))
#define TRANSFER_SIZE 64U         /* Transfer dataSize */
#define TRANSFER_BAUDRATE 500000U /* Transfer baudrate - 500k */

/*******************************************************************************
 * Prototypes
 ******************************************************************************/
/* LPSPI user SignalEvent */
void LPSPI_MasterSignalEvent_t(uint32_t event);

/*******************************************************************************
 * Variables
 ******************************************************************************/
AT_NONCACHEABLE_SECTION_INIT(uint8_t masterRxData[TRANSFER_SIZE]) = {0};
AT_NONCACHEABLE_SECTION_INIT(uint8_t masterTxData[TRANSFER_SIZE]) = {0};

volatile bool isTransferCompleted = false;
volatile bool isMasterOnTransmit = false;
volatile bool isMasterOnReceive = false;
/*******************************************************************************
 * Code
 ******************************************************************************/

uint32_t LPSPI3_GetFreq(void)
{
    return EXAMPLE_LPSPI_CLOCK_FREQ;
}
void LPSPI_MasterSignalEvent_t(uint32_t event)
{
    if (true == isMasterOnReceive)
    {
        PRINTF("This is LPSPI_MasterSignalEvent_t\r\n");
        PRINTF("Master receive data from slave has completed!\r\n");
        isMasterOnReceive = false;
    }
    if (true == isMasterOnTransmit)
    {
        PRINTF("This is LPSPI_MasterSignalEvent_t\r\n");
        PRINTF("Master transmit data to slave has completed!\r\n");
        isMasterOnTransmit = false;
    }
    isTransferCompleted = true;
}

/*!
 * @brief Main function
 */
int main(void)
{
    BOARD_ConfigMPU();
    BOARD_InitPins();
    BOARD_BootClockRUN();
    BOARD_InitDebugConsole();

    /*Set clock source for LPSPI*/
    CLOCK_SetMux(kCLOCK_LpspiMux, EXAMPLE_LPSPI_CLOCK_SOURCE_SELECT);
    CLOCK_SetDiv(kCLOCK_LpspiDiv, EXAMPLE_LPSPI_CLOCK_SOURCE_DIVIDER);

    PRINTF("LPSPI CMSIS driver board to board edma example.\r\n");
    PRINTF("This example use one board as master and another as slave.\r\n");
    PRINTF("Master and slave uses EDMA way. Slave should start first. \r\n");
    PRINTF("Please make sure you make the correct line connection. Basically, the connection is: \r\n");
    PRINTF("LPSPI_master -- LPSPI_slave   \r\n");
    PRINTF("   CLK       --    CLK  \r\n");
    PRINTF("   PCS       --    PCS \r\n");
    PRINTF("   SOUT      --    SIN  \r\n");
    PRINTF("   SIN       --    SOUT \r\n");
    PRINTF("   GND       --    GND \r\n");

    /* DMA Mux init and EDMA init */
    edma_config_t edmaConfig = {0};
    EDMA_GetDefaultConfig(&edmaConfig);
    EDMA_Init(EXAMPLE_LPSPI_MASTER_DMA_BASEADDR, &edmaConfig);
#if (defined(FSL_FEATURE_SOC_DMAMUX_COUNT) && FSL_FEATURE_SOC_DMAMUX_COUNT)
    DMAMUX_Init(EXAMPLE_LPSPI_MASTER_DMA_MUX_BASEADDR);
#endif
    uint32_t errorCount;
    uint32_t loopCount = 1U;
    uint32_t i;

    /*LPSPI master init*/
    DRIVER_MASTER_SPI.Initialize(LPSPI_MasterSignalEvent_t);
    DRIVER_MASTER_SPI.PowerControl(ARM_POWER_FULL);
    DRIVER_MASTER_SPI.Control(ARM_SPI_MODE_MASTER, TRANSFER_BAUDRATE);

    while (1)
    {
        /* Set up the transfer data */
        for (i = 0U; i < TRANSFER_SIZE; i++)
        {
            masterTxData[i] = (i + loopCount) % 256U;
            masterRxData[i] = 0U;
        }

        /* Print out transmit buffer */
        PRINTF("\r\n Master transmit:\r\n");
        for (i = 0; i < TRANSFER_SIZE; i++)
        {
            /* Print 16 numbers in a line */
            if ((i & 0x0FU) == 0U)
            {
                PRINTF("\r\n");
            }
            PRINTF(" %02X", masterTxData[i]);
        }
        PRINTF("\r\n");

        isTransferCompleted = false;
        isMasterOnTransmit = true;
        /* Start master transfer, send data to slave */
        DRIVER_MASTER_SPI.Send(masterTxData, TRANSFER_SIZE);
        /* Wait until transfer completed */
        while (!isTransferCompleted)
        {
        }

        /* Delay to wait slave is ready */
        for (i = 0U; i < EXAMPLE_LPSPI_DEALY_COUNT; i++)
        {
            __NOP();
        }

        isTransferCompleted = false;
        isMasterOnReceive = true;
        /* Start master transfer, receive data from slave */
        DRIVER_MASTER_SPI.Receive(masterRxData, TRANSFER_SIZE);
        /* Wait until transfer completed */
        while (!isTransferCompleted)
        {
        }

        errorCount = 0;
        for (i = 0; i < TRANSFER_SIZE; i++)
        {
            if (masterTxData[i] != masterRxData[i])
            {
                errorCount++;
            }
        }
        if (errorCount == 0)
        {
            PRINTF(" \r\nLPSPI transfer all data matched! \r\n");
            /* Print out receive buffer */
            PRINTF("\r\n Master received:\r\n");
            for (i = 0; i < TRANSFER_SIZE; i++)
            {
                /* Print 16 numbers in a line */
                if ((i & 0x0FU) == 0U)
                {
                    PRINTF("\r\n");
                }
                PRINTF(" %02X", masterRxData[i]);
            }
            PRINTF("\r\n");
        }
        else
        {
            PRINTF(" \r\nError occured in LPSPI transfer ! \r\n");
        }

        /* Wait for input any key */
        PRINTF("\r\n Input any char to run again\r\n");
        GETCHAR();
        /* Increase loop count to change transmit buffer */
        loopCount++;
    }
}
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
0 项奖励
回复

4,793 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jack,

You can find the SPI configurations with DRIVER_MASTER_SPI:


-> #define DRIVER_MASTER_SPI Driver_SPI3   

->pastedImage_1.png

->

pastedImage_3.png

Then run into the functions , you will find SPI configuration in detail .

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复