Update DMA source buffer before software trigger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update DMA source buffer before software trigger

Jump to solution
3,887 Views
r_poelstra
Contributor II

Hi,

I've configured a USART TX DMA channel (using the graphical config tool) that I trigger from software when bytes are available to be transmitted using:

DMA_DoChannelSoftwareTrigger(DMA0_DMA_BASEADDR, DMA0_LOG_UART_DMA_CHANNEL);

This works fine, but only with a fixed number of bytes each trigger.

How can I update the DMA channel so it knows how many bytes it should transfer?

 

Thanks in advance.

Kind regards,

 

Remco Poelstra

 

0 Kudos
Reply
1 Solution
3,862 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Remco Poelstra,

Yes, the DMA only can transfer fixed number of bits.

And a ring buffer DMA maybe suit for you , there is demo"lpcxpresso845max_usart_transfer_rb_dma" under SDK, you can have a look.

 

Regards,

Alice

 

View solution in original post

0 Kudos
Reply
4 Replies
3,837 Views
r_poelstra
Contributor II

Thanks for the reply.

I'll look into the ring buffer example. It might indeed be what I need.

 

Kind regards,

 

Remco Poelstra

 

0 Kudos
Reply
3,863 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Remco Poelstra,

Yes, the DMA only can transfer fixed number of bits.

And a ring buffer DMA maybe suit for you , there is demo"lpcxpresso845max_usart_transfer_rb_dma" under SDK, you can have a look.

 

Regards,

Alice

 

0 Kudos
Reply
3,870 Views
r_poelstra
Contributor II

Hi,

 

I'm using LPC844.

Kind regards,

 

Remco Poelstra

 

0 Kudos
Reply
3,873 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

Please let us know your chip part number, thus we can assign right engineer for your issue.

Thanks,

Jun Zhang

0 Kudos
Reply