USB Generic HID Device Example Code - What is the benefit of enabling the double buffer?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Generic HID Device Example Code - What is the benefit of enabling the double buffer?

1,757 Views
nbgatgi
Contributor IV

I'm using the LPCXpresso54608 SDK for MCUXpresso.  In particular, I'm running the generic HID device with FreeRTOS example code (link to my code/setup).

One of the settings is to enable the double buffer in usb_device_lpcip3511.h:

#define USB_DEVICE_IP3511_DOUBLE_BUFFER_ENABLE (1u)

The double buffer is enabled by default.  It seems to add a layer of complexity that I'm not sure I need, and I'm not so sure it is even working correctly with the example!

Could someone enlighten me on the purpose/intended use of the double buffer?

2 Replies

1,533 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Nick:

Double buffering is used for more efficient transfers.

Data in one buffer are being processed while the next set of data is read into the other one.

I hope it helps.

Regards

Daniel

0 Kudos
Reply

1,533 Views
nbgatgi
Contributor IV

I should have been more clear in my question.  I generally understand the purpose of double-buffering.  I'm looking for more of a walk-through of this particular implementation.  I can see the buffer index toggle, and see that every packet received goes into the alternate buffer, but within "USB_DeviceHidGenericCallback", the case "kUSB_DeviceHidEventRecvResponse" first calls "USB_DeviceHidSend" without toggling the buffer index, which echoes the data received the the IN-ENDPOINT (to the PC).  Right after that, the buffer index is toggled which generally makes sense to me.  THEN "USB_DeviceHidRecv" is called using the newly toggled buffer index.  WHAT IS THIS DOING?!?!

0 Kudos
Reply