Hello,
I am trying to port a KDS3.X/SDK2.X K64 project to MCUXpresso 10.3.X and SDK 2.5.
I noticed the device drivers have been changed on many peripherals, quite a few device driver APIs used in my project's APP need to be updated to the latest device drivers, mainly API naming.
I have done all that, then find out UART related APIs are not working properly. I am using an UART port for a terminal interface application.
I can use a UART directly with UART_Init(_UART, &config, CLOCK_GetFreq(_UART_CLK_SRC)), and
UART_WriteBlocking(_UART, txbuff, sizeof(txbuff) - 1)
But I cannot use:
DbgConsole_Init((uint8_t )_UART, 115200, DEBUG_CONSOLE_DEVICE_TYPE_UART, CLOCK_GetBusClkFreq());
and printf().
Shown in above screenshot, if I un-define DEBUG_CONSOLE_UART, the code can be stepped to API function
UART_WriteBlocking(_UART, txbuff, sizeof(txbuff) - 1) without any issue, but I do not want to do that since I have to create my only printf/scanf.
If I define DEBUG_CONSOLE_UART as shown in the above screenshot, when I stepped into line 96:
UART_EnableInterrupts(_UART, kUART_RxDataRegFullInterruptEnable | kUART_RxOverrunInterruptEnable);
it will generate a hard fault. I have used BDM to check both base and mask information is correctly pass to the function, and I have no clue why a hard fault will be generated right at the cursor highlight line.
I was thinking that may be related to how the project was created with different configurations, library files. After tried to create a few test projects with different configurations I still have the same issue.
Here is one of my project settings:
1. Project created.
2. Configuration (I almost tried all of the library files)
I am wondering if somebody else has seen this problem as well.
Hi Daniel,
I just noticed that the first passing parameter in the function DbgConsole_Init() has been changed as Daniel pointed out. I am wondering what is the parameter "instance", and wondering if it is the UART #, but I cannot find any example in SDK_2.5.0_TWR-K64F120M\boards\twrk64f120m\driver_examples\uart, using the function.
status_t DbgConsole_Init(uint32_t baseAddr, uint32_t baudRate, uint8_t device, uint32_t clkSrcFreq)
status_t DbgConsole_Init(uint8_t instance, uint32_t baudRate, serial_port_type_t device, uint32_t clkSrcFreq)
It is kind of inconsistent to update the device driver with the same name but change to different parameters.
Thanks,
Zhiqun
Please also refer to the uart demo.
SDK_2.5.0_TWR-K64F120M\boards\twrk64f120m\driver_examples\uart
Regards
Daniel
Hi Zhiqun:
The reason of the hard fault maybe because the uart clock is not enabled, could you please check with it?
I would suggest you step into the DbgConsole_Init. The implementation of DbgConsole_Init in SDK2.5 is totally different from your old sdk. I am assuming you are using SDK 2.2 or 2.3.
The old implementation is :
/* See fsl_debug_console.h for documentation of this function. */
status_t DbgConsole_Init(uint32_t baseAddr, uint32_t baudRate, uint8_t device, uint32_t clkSrcFreq)
{
if (s_debugConsole.type != DEBUG_CONSOLE_DEVICE_TYPE_NONE)
{
return kStatus_Fail;
}
/* Set debug console to initialized to avoid duplicated initialized operation. */
s_debugConsole.type = device;
/* Switch between different device. */
switch (device)
{
#if (defined(FSL_FEATURE_SOC_UART_COUNT) && (FSL_FEATURE_SOC_UART_COUNT > 0)) || \
(defined(FSL_FEATURE_SOC_IUART_COUNT) && (FSL_FEATURE_SOC_IUART_COUNT > 0))
case DEBUG_CONSOLE_DEVICE_TYPE_UART:
case DEBUG_CONSOLE_DEVICE_TYPE_IUART:
........
In SDK 2.5,
/* See fsl_debug_console.h for documentation of this function. */
status_t DbgConsole_Init(uint8_t instance, uint32_t baudRate, serial_port_type_t device, uint32_t clkSrcFreq)
{
serial_manager_config_t serialConfig;
status_t status = kStatus_SerialManager_Error;
#if (defined(SERIAL_PORT_TYPE_UART) && (SERIAL_PORT_TYPE_UART > 0U))
serial_port_uart_config_t uartConfig = {
.instance = instance,
.clockRate = clkSrcFreq,
.baudRate = baudRate,
.parityMode = kSerialManager_UartParityDisabled,
.stopBitCount = kSerialManager_UartOneStopBit,
.enableRx = 1,
.enableTx = 1,
};
#endif
#if (defined(SERIAL_PORT_TYPE_USBCDC) && (SERIAL_PORT_TYPE_USBCDC > 0U))
serial_port_usb_cdc_config_t usbCdcConfig = {
.controllerIndex = (serial_port_usb_cdc_controller_index_t)instance,
};
#endif
.......
The input parameter is different,
In sdk2.2
status_t DbgConsole_Init(uint32_t baseAddr, uint32_t baudRate, uint8_t device, uint32_t clkSrcFreq)
In sdk 2.5
/* See fsl_debug_console.h for documentation of this function. */
status_t DbgConsole_Init(uint8_t instance, uint32_t baudRate, serial_port_type_t device, uint32_t clkSrcFreq)
I hope it helps
Regards
Daniel