ThreadX + NetX example for iMXRT1010

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ThreadX + NetX example for iMXRT1010

1,406 Views
Hiren_Bhuva
Contributor I

Hello Community,

We are working on a project  which uses ThreadX + NetX Code in the application. we have LTE module in our product. So, we do not need ethernet in our application . However we need network stack.

We need to port the application to iMXRT1010 MCU.

We tried to find NetX demo in the MCU Xpresso SDK. But, we  are not able to find any example for the same. We are using SDK generated from Here  .

Can you help us to find the example code for the same.

Thanks,

Hiren Bhuba

Tags (1)
0 Kudos
Reply
1 Reply

1,390 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Hiren_Bhuva,

RT1010 hasn't ENET interface, so its SDK hasn't ethernet example. You can download RT1060 SDK. It has threadx example and netX example in azure_rtos_examples folder. But you have to port these examples to RT1010.

 

Regards,

Jing

0 Kudos
Reply