SDK for MKW41Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK for MKW41Z

3,192 Views
aditihilbert
Contributor I

Building a SDK for the MKW41Z

I am trying to build or download V2.0 of the Kinetis SDK. I have v1.3 and they have the MKW40Z but not the 41Z. When I went to the SDK builder there is no option for the KW41Z. Someone know where to get this?

 

Thanks!

Labels (1)
0 Kudos
Reply
3 Replies

2,689 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Aditi Hilbert

Please check the following link:

ARM Cortex-M0+|Kinetis KW41Z 2.4 GHz 32-bit MCUs|NXP 

you can find the SDK support in the Kinetis KW41Z Connectivity Software in the Protocol Stacks tab

Regards

Jorge Alcala

0 Kudos
Reply

2,689 Views
aditihilbert
Contributor I

Hi Jorge,

I got it. It was the link right below the one I looked at first :smileyhappy:

thanks!

0 Kudos
Reply

2,689 Views
aditihilbert
Contributor I

This is not what I need. This is an .exe and I am doing development on OSX. I can use the 40Z stuff for now, but I would have thought that the 41Z is supported as well but I cannot find it in v1.3. If there is a comprehensive 2.0 SDK download somewhere that contains the 41Z that would be great!

0 Kudos
Reply