SAI/I2S Example for FRDM-K64f

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SAI/I2S Example for FRDM-K64f

2,031件の閲覧回数
nteschner
Contributor I

Hi,

i'm using the FRDM-K64F Board and try to connect it via I2S to an external I2S Microphone:

  1. Are there any SAI Examples for this board?
  2. Or maybe Example for similar Board, such i could addept it for the FRDM-K64f?


I know from the SDK documentation that there should be examples for other boards. Any suggestions which Example from which other Board i could use?

Best

ラベル(1)
0 件の賞賛
返信
1 返信

1,968件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The attachment is the twr-k60's i2s. You can refer it.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信