Request for Simplified Sample Code for FlexCAN and CAN FD on RT1170EVKB Board for MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request for Simplified Sample Code for FlexCAN and CAN FD on RT1170EVKB Board for MCUXpresso IDE

1,841件の閲覧回数
Govind89
Contributor II
 
I am a beginner with the RT1170 controller. We have an RT1170EVKB board and need a simple sample source code for FlexCAN and CAN FD for the MCUXpresso IDE. The provided examples are difficult for me to understand. Could you please provide simple source code? This will help me study and better understand the default sample code.
 

Thank you

0 件の賞賛
返信
4 返答(返信)

937件の閲覧回数
Govind89
Contributor II

Sorry for the delay. I am using this example as a reference to ensure successful communication. Thank you for your support.

0 件の賞賛
返信

1,825件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Govind89 ,

Thanks for your interest in NXP MIMXRT series!

Example demos for both FlexCAN and CANFD are present in the SDK. You can build and download the SDK here:Select Board | MCUXpresso SDK Builder (nxp.com)

Gavin_Jia_0-1718357423500.png

Import the SDK in MCUXpressoIDE and then import the demos you need:

Gavin_Jia_1-1718357528800.png

Or use Keil/IAR to open the extracted project.

 

Best regards,
Gavin

 

0 件の賞賛
返信

1,811件の閲覧回数
Govind89
Contributor II

Thank you for your response. I have already reviewed the examples provided. However, could you please supply basic beginner-level source code for CAN?

0 件の賞賛
返信

1,771件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Govind89 ,

The FlexCAN routines provided with the SDK, include two types, one is self-sending and self-receiving loopback, and the other is sending/receiving data frames from the CAN bus. If you are referring to the second type and need to build a CAN bus network, it is best to have a CAN protocol analyzer. This will allow you to see the data transmitted on the CAN bus.

A transmitting node on the CAN bus, if it sends a data frame out and there is no answer on the bus, it will continue to send the same data frame until the error accumulates to 255 and the bus freezes the node. So it is recommended to debug the CAN code and configure a CAN protocol analyzer that will make the CAN bus node send a data frame and always get an answer frame.

Starting with the simplest loopback should be a nice start.

Best regards,
Gavin

Gavin_Jia_0-1718617216043.png