I'm currently building a C++ application on the RW612. I tried defining vApplicationTickHook() in my application but got a message that it was already defined in wifi/port/osa/osa_freertos.c. OK, that's fine... I can see you provide an API function OSA_SetupTickFunction() to add custom tick functions. So I add the following code to my C++ module:
#include <osa.h>
extern "C" {
void Program_ApplicationTickHook(void) {
Clock_Update(os_get_ticks());
}
} // extern "C"
namespace ls {
AppInitResult Program::Stage1Init(void) {
OSA_SetupTickFunction(&Program_ApplicationTickHook);
return AppInitResult::kOk;
}
} // namespace lsAnd that compiles just fine. But then the linker throws an error:
C:\NXP\workspace\my_project\Debug/../source/program.cpp:45:(.text._ZN2ls7Program10Stage1InitEv+0xa): undefined reference to `OSA_SetupTickFunction(void (*)())'Wait, what? I can see that function in osa_freertos.c. Then I check something... there are no C++ guards in your Wi-Fi stack software, anywhere. I change my code to read:
extern "C" {
#include <osa.h>
}And now the code links correctly, because the C++ compiler knows not to mangle the names of plain C functions.
It is unacceptable for a vendor to provide SDK C code that is not C++ ready. Please fix this issue in your Wi-Fi stack code, and all other NXP SDK components. (And be sure to properly surround type declarations and externs as well, not just function declarations.) Thank you.
Dana M.
Hi,
I'm sorry for the inconvenience.
I'll pass your comments to the corresponding team.
Regards,
Daniel.