RT1170EVKB USB-RNDIS automatic recognition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1170EVKB USB-RNDIS automatic recognition

Jump to solution
1,611 Views
seobi
Contributor III


Hi, I successfully communicated with a Windows PC using the VNIC sample and lwIP sample on the RT1170EVKB.

However, to enable communication on the Windows PC, I had to install the "fsl_rndis.inf" file for the Ethernet device to be created.

The issue is that this works on Windows, but I'm not sure how to use the RNDIS functionality on Linux (such as Ubuntu).

I hope RNDIS will be automatically recognized by all operating systems.

Is there a way to enable RNDIS mode on operating systems other than Windows, such as Linux?

Best regards,

0 Kudos
Reply
1 Solution
1,590 Views
seobi
Contributor III

I have confirmed that the Ethernet device is automatically recognized on UBUNTU.

I would like to cancel this question.

Best regards,

View solution in original post

0 Kudos
Reply
1 Reply
1,590 Views
seobi
Contributor III

I have confirmed that the Ethernet device is automatically recognized on UBUNTU.

I would like to cancel this question.

Best regards,

0 Kudos
Reply