RT1064 lwip_httpssrv_mbedTLS_freertos

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1064 lwip_httpssrv_mbedTLS_freertos

1,014 次查看
newtofourms
Contributor I

Hello,

 

So started to mess around with mbedTLS on the RT1064-EVK and the lwip_httpssrv_mbedTLS_freertos example implementation doesn't seem to work. I get a site can't be reached error but the SSL certificate is being served. If you were to disable mbedTLS in the pre-processor config and try to access over http, it works. Additionally the lwip_httpssrv_mbedTLS_bm example works too. Any ideas what could be wrong??

Attached below is the project file.

 

 

0 项奖励
回复
1 回复

1,000 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi

This is an issue for FreeRTOS MCUXpresso debug target. It will be fixed in next release.  It works for the release target. 

Also works for IAR or Keil.

 

 

Regards

Daniel

 

0 项奖励
回复