Question of the "flexcan_pretended_networking_wakeup" about frdmmcxn236

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question of the "flexcan_pretended_networking_wakeup" about frdmmcxn236

324 Views
yhc123
Contributor II

I'm looking the "flexcan_pretended_networking_wakeup" case of SDK_25_03_00_FRDM-MCXN236, and I want to know what's the meaning of wake up payload range in the readme file, 0x0055000000000000 seems like a 64bit data but the platfporm just 32bits.

yhc123_1-1750164307603.png

 

Does the payload for sending data need to be between 0x00550000000000 and 0x005600000000000 for the receiving end to receive it? Why receiving end can reveive the match message 2 and  match message 1, they are out of range maybe.

yhc123_0-1750164281288.png

 

0 Kudos
Reply
1 Reply

285 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @yhc123,

The wake-up payload range is set as an example of how to define a range for the pretended device to be woken up. However, this is only an illustrative method, as it is not actually used on the wakeup procedure. In the example, as long as 4 messages are received, the device will wake-up.

BR,
Edwin.

0 Kudos
Reply