Please provide MCUXpresso SDK API Reference Manual document

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Please provide MCUXpresso SDK API Reference Manual document

ソリューションへジャンプ
9,397件の閲覧回数
anaseem
Contributor IV

Please provide MUCXpresso SDK API Reference Manual document (MCUXSDKAPIRM).  It is referenced in "Getting Started with MCUXpresso SDK.pdf."

ラベル(1)
タグ(1)
1 解決策
8,935件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Amer,

I attached it for you.

You can also download SDK package and Docs from: https://mcuxpresso.nxp.com/en/select    


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
8,588件の閲覧回数
superaga
Contributor III

Hi NXP,

I'm using the latest MCUXpresso 11.3.0.

I installed the SDK_2.9.0_FRDM-K64F for which I'd like to access to the API documentation.

I read the above answer, but it doesn't solve the issue.

I can open the SDK Getting started or the Release notes from:

  • within the MCUXpresso IDE or
  • from the docs folder inside the SDK.

superaga_0-1612997782816.png

Unfortunately none of the 2 point me to the SDK documentation. I found it just using Google a this address but of course I think there is a better way to access to the official documentation. What is it?

One more, I think that would be very appreciated been able to open the SDK html (exist?!?) from within the MCUXpresso IDE.

Would be also very useful use the context menu over a function to open directly the function doc (I suppose the SDK is done with the Doxygen).

 

Many thanks!

Kind regards,

AGA

0 件の賞賛
返信
8,934件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Amer Naseem,

You can find it under SDK package->docs after you download SDK.

Or you can tell me which chip you use, I will send it for you.

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

8,935件の閲覧回数
anaseem
Contributor IV

imX8.PNG

0 件の賞賛
返信
8,936件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Amer,

I attached it for you.

You can also download SDK package and Docs from: https://mcuxpresso.nxp.com/en/select    


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------