Please provide MCUXpresso SDK API Reference Manual document

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Please provide MCUXpresso SDK API Reference Manual document

跳至解决方案
7,179 次查看
anaseem
Contributor IV

Please provide MUCXpresso SDK API Reference Manual document (MCUXSDKAPIRM).  It is referenced in "Getting Started with MCUXpresso SDK.pdf."

标签 (1)
标记 (1)
1 解答
6,718 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Amer,

I attached it for you.

You can also download SDK package and Docs from: https://mcuxpresso.nxp.com/en/select    


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
6,371 次查看
superaga
Contributor III

Hi NXP,

I'm using the latest MCUXpresso 11.3.0.

I installed the SDK_2.9.0_FRDM-K64F for which I'd like to access to the API documentation.

I read the above answer, but it doesn't solve the issue.

I can open the SDK Getting started or the Release notes from:

  • within the MCUXpresso IDE or
  • from the docs folder inside the SDK.

superaga_0-1612997782816.png

Unfortunately none of the 2 point me to the SDK documentation. I found it just using Google a this address but of course I think there is a better way to access to the official documentation. What is it?

One more, I think that would be very appreciated been able to open the SDK html (exist?!?) from within the MCUXpresso IDE.

Would be also very useful use the context menu over a function to open directly the function doc (I suppose the SDK is done with the Doxygen).

 

Many thanks!

Kind regards,

AGA

0 项奖励
回复
6,717 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Amer Naseem,

You can find it under SDK package->docs after you download SDK.

Or you can tell me which chip you use, I will send it for you.

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

6,718 次查看
anaseem
Contributor IV

imX8.PNG

0 项奖励
回复
6,719 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Amer,

I attached it for you.

You can also download SDK package and Docs from: https://mcuxpresso.nxp.com/en/select    


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------