MIMXRT1170-EVK FreeRTOS Hello Example Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1170-EVK FreeRTOS Hello Example Issue

132件の閲覧回数
Rosh
Contributor I

Hi Team,

I imported the evkbmimxrt1170_freertos_hello_cm7 example project from the MCUXpresso SDK into MCUXpresso IDE without making any significant modifications.

The project builds successfully without any errors or warnings and downloads to the MIMXRT1170-EVK(MIMXRT1176DVMAA) board successfully.

The task created successfully and executes only once and then stops at address 0xDEADBEEE. This behavior occurs every time.

LED Toggle Task:

To verify whether the problem was related to vTaskSuspend(), I've created another task with a simple LED blinking task.

Expected behavior:

  • LED should toggle every 100 ms continuously.

Actual behavior:

  • LED toggles only once.
  • After the first execution, debugger again stops at: 0xDEADBEEE

Kindly clarify the following queries,

  • What does address 0xDEADBEEE indicate in the MCUXpresso SDK for i.MX RT1170?
  • Why does the task execute only once instead of running periodically?
  • Is there any additional configuration required to work correctly on the MIMXRT1170-EVK?
  • What changes are required to make the task execute periodically as expected?

Rosh_0-1786093292545.pngRosh_1-1786093311524.pngRosh_2-1786093339102.png

 

 

タグ(1)
0 件の賞賛
返信
2 返答(返信)

104件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

Hello @Rosh,
I understand that you are currently using the MIMXRT1170-EVK. Please note that the SDK for the MIMXRT1170-EVK is different from the SDK provided for the MIMXRT1170-EVKB. Could you please download and test with the SDK specifically generated for the RT1170-EVK using the MCUXpresso SDK Builder?

Habib_MS_0-1786125239179.png

I understand your point. The SDK examples are intended to provide a common use cases for each peripheral functionality. The 0xDEADBEE value is typically associated with a HardFault condition.
Could you please run the example without any modifications and let me know the results using the latest available SDK version?

BR
Habib

0 件の賞賛
返信

59件の閲覧回数
Rosh
Contributor I

Hi @Habib_MS 

I've downloaded the SDK specifically generated for the RT1170-EVK using the MCUXpresso SDK Builder and tested it. It is working fine now.

Thank you for your support.

0 件の賞賛
返信