Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux

1,682 Views
davidmccall
Contributor I

Can I run Linux on LPCXpresso 54286? , if so where can I download?
thanks in advance.

0 Kudos
Reply
1 Reply

1,510 Views
soledad
NXP Employee
NXP Employee

Hi,

What do you mean by LPCXpresso 54286?

In the following link you will find how to installing LPCXpresso on Linux

Installing LPCXpresso on Linux 

MCUXpresso IDE is now recommended for developers using LPC Cortex-M based microcontrollers. This IDE offers a fully feature development environment for both LPC and Kinetis Cortex-M based microcontrollers which fully supports LPCOpen and MCUXpresso SDK. For more details of MCUXpresso IDE, please visithttp://www.nxp.com/mcuxpresso/ide

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply