LPC546xx - CLOCK_GetFlexCommClkFreq - Error report

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC546xx - CLOCK_GetFlexCommClkFreq - Error report

1,449 次查看
guillaume-b
Contributor I

I would like to report an error in "CLOCK_GetFlexCommClkFreq function" of "fsl_clock.c" for LPC546xx.

Below my correction :

/* Get FLEXCOMM Clk */
uint32_t CLOCK_GetFlexCommClkFreq(uint32_t id)
{
    return (SYSCON->FCLKSEL[id] == 0U) ? CLOCK_GetFro12MFreq() :
           (SYSCON->FCLKSEL[id] == 1U) ? CLOCK_GetFroHfFreq() :
           //(SYSCON->FCLKSEL[id] == 2U) ? CLOCK_GetPllOutFreq()  : // original error !!!
           //(SYSCON->FCLKSEL[id] == 3U) ? CLOCK_GetI2SMClkFreq() : // original error !!!
           (SYSCON->FCLKSEL[id] == 2U) ? CLOCK_GetAudioPllOutFreq() : // my correction
           (SYSCON->FCLKSEL[id] == 3U) ? CLOCK_GetMclkClkFreq() : // my correction
           (SYSCON->FCLKSEL[id] == 4U) ? CLOCK_GetFreq(kCLOCK_Frg) : 0U;
}

Reference : UM10912 -> 7.5.37 Flexcomm Interface clock source select registers

标记 (1)
0 项奖励
回复
1 回复

1,233 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi BOSSARD Guillaume,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

Thanks for your reporting, and I'll transfer it to SDK software team.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复