Kinetis SDK examples - Design Patterns

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis SDK examples - Design Patterns

ソリューションへジャンプ
1,285件の閲覧回数
thilankadamith
Contributor I

Hi,

I'm curious to know about the design pattern used in the Kinetis SDK examples so that I can customize the code easily. For example in the bootloader code, all the interfaces defined by structures, implementations are mapped in various .c files (memory.c, bl_tree_root.c, property_kinetis.c) and then called in bl_main.c
Where can I find more information about design patterns used in Kinetis SDK examples and any best practices for NXP Kinetis MCUs?

example -

In bl_context.c

 

 

 

bootloader_context_t g_bootloaderContext = {.memoryInterface = &g_memoryInterface,
                                            .memoryMap = g_memoryMap,
#if BL_FEATURE_EXPAND_MEMORY
                                            .externalMemoryMap = g_externalMemoryMap,
#endif // BL_FEATURE_EXPAND_MEMORY
                                            .allPeripherals = g_peripherals,
                                            .activePeripheral = NULL, // Filled in at run time.
                                            .propertyInterface = &g_propertyInterface,
                                            .commandInterface = &g_commandInterface,
#if !BL_FEATURE_HAS_NO_INTERNAL_FLASH
                                            .flashDriverInterface = &g_flashDriverInterface,
#if !BL_DEVICE_IS_LPC_SERIES
                                            .allFlashState = &g_flashState,
                                            .allFlashCacheState = &g_flashcacheState,
#if BL_FEATURE_SUPPORT_DFLASH
                                            .dflashDriverInterface = &g_dflashDriverInterface,
                                            .dFlashState = &g_dflashState,
#endif // BL_FEATURE_SUPPORT_DFLASH
                                            
#else
                                            .allFlashState = g_flashState,
#endif // !BL_DEVICE_IS_LPC_SERIES
#endif // #if !BL_FEATURE_HAS_NO_INTERNAL_FLASH
#if AES_SECURITY_SUPPORTED
                                            .aesInterface = &g_aesInterface,
#endif

};

 

 

 

In bl_main.c

 

 

   // Init the active peripheral.
    if (g_bootloaderContext.activePeripheral->byteInterface &&
        g_bootloaderContext.activePeripheral->byteInterface->init)
    {
        g_bootloaderContext.activePeripheral->byteInterface->init(g_bootloaderContext.activePeripheral);
    }
    if (g_bootloaderContext.activePeripheral->packetInterface &&
        g_bootloaderContext.activePeripheral->packetInterface->init)
    {
        g_bootloaderContext.activePeripheral->packetInterface->init(g_bootloaderContext.activePeripheral);
    }

 

 

Thank you in advance.

0 件の賞賛
返信
1 解決策
1,267件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

This information can be found on the SDK documentation. You can download this at this page: https://mcuxpresso.nxp.com/en/welcome.

Let me know if this is helpful, if you have more questions do not hesitate to ask me.
Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,268件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

This information can be found on the SDK documentation. You can download this at this page: https://mcuxpresso.nxp.com/en/welcome.

Let me know if this is helpful, if you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信