KW41Z BLE + Thread Application SDK Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW41Z BLE + Thread Application SDK Error

6,596件の閲覧回数
Athena
Contributor I

Hi, 

I have been trying to build the SDK example Hybrid BLE Thread Wireless router but I keep getting the same error. If anyone could help me troubleshoot the error as I need it done as soon as possible. 

Thank you. 

0 件の賞賛
返信
13 返答(返信)

6,587件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Please show me the detail of this  error.

error.PNG

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,572件の閲覧回数
Athena
Contributor I

Hello. 

Firstly, this is the error that would appear once I've debugged it 

Screenshot 2021-06-29 at 11.52.12 PM.png

 

And then looking into the details of the warning, pictures below shows the warning sign in the particular line. 

 

Screenshot 2021-06-29 at 11.57.28 PM.png

 

 

 

 

Screenshot 2021-06-29 at 11.57.36 PM.png

 

How do I solve this problem? So I can embed the BLE application to my board.

 

Thank you.

 

0 件の賞賛
返信

6,566件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The first picture says that the program file doesn't exist. Did you compile the program correctly?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,563件の閲覧回数
Athena
Contributor I

Hello, 

Previously this was my compiling settings. 

Screenshot 2021-06-30 at 1.05.30 PM.png

I have also tried to set it as the default compiler but unfortunately, still got the same error.

I also followed the steps in the tutorial carefully. 

0 件の賞賛
返信

6,555件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

When you press the button 'build', there will a compile log. Please show me that log. Do you use the latest sdk? Do you use the other ide to try the example?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,529件の閲覧回数
Athena
Contributor I

Hi.

I have attached a .docx file containing the compile log. Also, I am using the latest version of the SDK, 2.2.3

0 件の賞賛
返信

6,523件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

You didn't compile the program successfully, of course, you can't download the program.

Please check this error and modify it.

error.PNG

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,516件の閲覧回数
Athena
Contributor I

Hello, Sorry do you mind elaborating on that?

I am new to this so I appreciate if there would be more information on which error I should troubleshoot. 

Thank you!

0 件の賞賛
返信

6,511件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The picture I post has shown the error. In file 'mac_filtering.c', there is redundant character ' ` ' in file.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,509件の閲覧回数
Athena
Contributor I

Hello, thanks I've already removed it! However, there is still an error but I cannot decipher what it means. 

Athena_0-1625561385267.png

Athena_1-1625561405893.png

 

0 件の賞賛
返信

6,496件の閲覧回数
Athena
Contributor I

Hi. 

Yes, the log is attached below Also, I am using the latest SDK version 2.2.3 

-------------------------------------------------------------------------------------------------------

01:30:03 **** Build of configuration Debug for project frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble ****

make -r -j7 all 

Building file: ../startup/startup_MKW41Z4.S

Building file: ../nwk_ip/base/utils/mac_filtering.c

Invoking: MCU Assembler

arm-none-eabi-gcc -c -x assembler-with-cpp -D__REDLIB__ -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/board" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/CMSIS" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/OSAbstraction/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/freertos" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/mac/source/App" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/mac/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/phy/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/GPIO" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Keyboard/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/LED/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Source/SPI_Adapter" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Source/UART_Adapter" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Source/I2C_Adapter" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Flash/Internal" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/common" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/FSCI/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/FSCI/Source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/MemManager/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Messaging/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/LowPower/Interface/MKW41Z" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/LowPower/Source/MKW41Z" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Shell/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/NVM/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/NVM/Source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Panic/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/RNG/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/TimersManager/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/TimersManager/Source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SecLib" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Lists" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/FunctionLib" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/ModuleInfo" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/host/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/common" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/host/config" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/controller/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/hci_transport/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/common/gatt_db/macros" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/common/gatt_db" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/profiles/battery" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/profiles/device_info" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/profiles/wireless_uart" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/MWSCoexistence/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface/modules" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface/thread" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/base/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface/http" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/app/config" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/app/common" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/drivers" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/DCDC/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/XCVR/MKW41Z4" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/phy/source/MKW41Z" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/utilities" -g3 -mcpu=cortex-m0plus -mthumb -D__REDLIB__ -specs=redlib.specs -o "startup/startup_MKW41Z4.o" "../startup/startup_MKW41Z4.S"

Invoking: MCU C Compiler

arm-none-eabi-gcc -std=gnu99 -D__REDLIB__ -DCPU_MKW41Z512VHT4 -DCPU_MKW41Z512VHT4_cm0plus -D__SEMIHOST_HARDFAULT_DISABLE=1 -DFSL_RTOS_FREE_RTOS -DFRDM_KW41Z -DFREEDOM -DSDK_DEBUGCONSOLE=1 -DCR_INTEGER_PRINTF -DPRINTF_FLOAT_ENABLE=0 -D__MCUXPRESSO -D__USE_CMSIS -DDEBUG -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/board" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/CMSIS" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/OSAbstraction/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/freertos" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/mac/source/App" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/mac/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/phy/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/GPIO" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Keyboard/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/LED/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Source/SPI_Adapter" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Source/UART_Adapter" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Source/I2C_Adapter" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Flash/Internal" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/common" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/FSCI/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/FSCI/Source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/MemManager/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Messaging/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/LowPower/Interface/MKW41Z" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/LowPower/Source/MKW41Z" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Shell/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/NVM/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/NVM/Source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Panic/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/RNG/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/TimersManager/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/TimersManager/Source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SecLib" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Lists" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/FunctionLib" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/ModuleInfo" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/host/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/common" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/host/config" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/controller/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/hci_transport/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/common/gatt_db/macros" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/common/gatt_db" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/profiles/battery" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/profiles/device_info" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/profiles/wireless_uart" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/MWSCoexistence/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface/modules" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface/thread" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/base/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface/http" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/app/config" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/app/common" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/drivers" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/DCDC/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/XCVR/MKW41Z4" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/phy/source/MKW41Z" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/utilities" -Os -fno-common -g -Wall -Wno-missing-braces  -c  -ffunction-sections  -fdata-sections  -ffreestanding  -fno-builtin -imacros "/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/config.h" -fmacro-prefix-map="../nwk_ip/base/utils/"=. -mcpu=cortex-m0plus -mthumb -D__REDLIB__ -fstack-usage -specs=redlib.specs -MMD -MP -MF"nwk_ip/base/utils/mac_filtering.d" -MT"nwk_ip/base/utils/mac_filtering.o" -MT"nwk_ip/base/utils/mac_filtering.d" -o "nwk_ip/base/utils/mac_filtering.o" "../nwk_ip/base/utils/mac_filtering.c"

../nwk_ip/base/utils/mac_filtering.c:1:1: error: stray '`' in program

    1 | `/*

      | ^

../nwk_ip/base/utils/mac_filtering.c: In function 'MacFiltering_Active':

../nwk_ip/base/utils/mac_filtering.c:314:9: warning: converting a packed 'macFilteringDefault_t' {aka 'enum <anonymous>'} pointer (alignment 1) to a 'void *' pointer (alignment 4) may result in an unaligned pointer value [-Waddress-of-packed-member]

  314 |         NVNG_SyncSave((void **)&mbDefaultSetting);

      |         ^~~~~~~~~~~~~

In file included from ../nwk_ip/base/utils/mac_filtering.c:23:

/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/base/interface/mac_filtering.h:38:1: note: defined here

   38 | {

      | ^

../nwk_ip/base/utils/mac_filtering.c: In function 'MacFiltering_Reset':

../nwk_ip/base/utils/mac_filtering.c:353:5: warning: converting a packed 'macFilteringDefault_t' {aka 'enum <anonymous>'} pointer (alignment 1) to a 'void *' pointer (alignment 4) may result in an unaligned pointer value [-Waddress-of-packed-member]

  353 |     NVNG_SyncSave((void **)&mbDefaultSetting);

      |     ^~~~~~~~~~~~~

In file included from ../nwk_ip/base/utils/mac_filtering.c:23:

/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/base/interface/mac_filtering.h:38:1: note: defined here

   38 | {

      | ^

make: *** [nwk_ip/base/utils/subdir.mk:32: nwk_ip/base/utils/mac_filtering.o] Error 1

make: *** Waiting for unfinished jobs....

Finished building: ../startup/startup_MKW41Z4.S

 

"make -r -j7 all" terminated with exit code 2. Build might be incomplete.

 

01:30:04 Build Failed. 3 errors, 2 warnings. (took 635ms)

0 件の賞賛
返信

6,496件の閲覧回数
Athena
Contributor I

Hello!

I have attached the log below. Yes, I used the latest version of SDK which is the 2.2.3 and what do you mean by other IDE? 

---------------------------------------------------------------------------------------------------------------------------------------------

04 **** Incremental Build of configuration Debug for project frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble ****

make -r -j7 all 

Building file: ../nwk_ip/base/utils/mac_filtering.c

Invoking: MCU C Compiler

arm-none-eabi-gcc -std=gnu99 -D__REDLIB__ -DCPU_MKW41Z512VHT4 -DCPU_MKW41Z512VHT4_cm0plus -D__SEMIHOST_HARDFAULT_DISABLE=1 -DFSL_RTOS_FREE_RTOS -DFRDM_KW41Z -DFREEDOM -DSDK_DEBUGCONSOLE=1 -DCR_INTEGER_PRINTF -DPRINTF_FLOAT_ENABLE=0 -D__MCUXPRESSO -D__USE_CMSIS -DDEBUG -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/board" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/CMSIS" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/OSAbstraction/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/freertos" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/mac/source/App" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/mac/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/phy/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/GPIO" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Keyboard/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/LED/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Source/SPI_Adapter" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Source/UART_Adapter" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Source/I2C_Adapter" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Flash/Internal" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/common" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/FSCI/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/FSCI/Source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/MemManager/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Messaging/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/LowPower/Interface/MKW41Z" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/LowPower/Source/MKW41Z" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Shell/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/NVM/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/NVM/Source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Panic/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/RNG/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SerialManager/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/TimersManager/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/TimersManager/Source" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/SecLib" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/Lists" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/FunctionLib" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/ModuleInfo" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/host/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/common" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/host/config" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/controller/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/hci_transport/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/common/gatt_db/macros" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/common/gatt_db" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/profiles/battery" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/profiles/device_info" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/bluetooth/profiles/wireless_uart" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/MWSCoexistence/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface/modules" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface/thread" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/base/interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/core/interface/http" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/app/config" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/app/common" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/drivers" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/DCDC/Interface" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/framework/XCVR/MKW41Z4" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/ieee_802.15.4/phy/source/MKW41Z" -I"/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/utilities" -Os -fno-common -g -Wall -Wno-missing-braces  -c  -ffunction-sections  -fdata-sections  -ffreestanding  -fno-builtin -imacros "/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/source/config.h" -fmacro-prefix-map="../nwk_ip/base/utils/"=. -mcpu=cortex-m0plus -mthumb -D__REDLIB__ -fstack-usage -specs=redlib.specs -MMD -MP -MF"nwk_ip/base/utils/mac_filtering.d" -MT"nwk_ip/base/utils/mac_filtering.o" -MT"nwk_ip/base/utils/mac_filtering.d" -o "nwk_ip/base/utils/mac_filtering.o" "../nwk_ip/base/utils/mac_filtering.c"

../nwk_ip/base/utils/mac_filtering.c:1:1: error: stray '`' in program

    1 | `/*

      | ^

../nwk_ip/base/utils/mac_filtering.c: In function 'MacFiltering_Active':

../nwk_ip/base/utils/mac_filtering.c:314:9: warning: converting a packed 'macFilteringDefault_t' {aka 'enum <anonymous>'} pointer (alignment 1) to a 'void *' pointer (alignment 4) may result in an unaligned pointer value [-Waddress-of-packed-member]

  314 |         NVNG_SyncSave((void **)&mbDefaultSetting);

      |         ^~~~~~~~~~~~~

In file included from ../nwk_ip/base/utils/mac_filtering.c:23:

/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/base/interface/mac_filtering.h:38:1: note: defined here

   38 | {

      | ^

../nwk_ip/base/utils/mac_filtering.c: In function 'MacFiltering_Reset':

../nwk_ip/base/utils/mac_filtering.c:353:5: warning: converting a packed 'macFilteringDefault_t' {aka 'enum <anonymous>'} pointer (alignment 1) to a 'void *' pointer (alignment 4) may result in an unaligned pointer value [-Waddress-of-packed-member]

  353 |     NVNG_SyncSave((void **)&mbDefaultSetting);

      |     ^~~~~~~~~~~~~

In file included from ../nwk_ip/base/utils/mac_filtering.c:23:

/Users/camillemavic/Documents/MCUXpressoIDE_11.3.0/workspace/frdmkw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_ble/nwk_ip/base/interface/mac_filtering.h:38:1: note: defined here

   38 | {

      | ^

make: *** [nwk_ip/base/utils/subdir.mk:32: nwk_ip/base/utils/mac_filtering.o] Error 1

"make -r -j7 all" terminated with exit code 2. Build might be incomplete.

 

17:39:04 Build Failed. 2 errors, 2 warnings. (took 796ms)

0 件の賞賛
返信

6,485件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

You can try to use IAR to compile the program.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信