K63 and ADC interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K63 and ADC interrupt

2,467 Views
darshan_shah1
Contributor II

I am using custom board with K63. I would like to use ADC interrupt to be triggered when value is less than threshold.

I have gone through ADC sample code and write my own ADC interrupt, yet I am not able to get ADC interrupt.

 

#define VBUS_ADC                            ADC1
#define VBUS_THRESH                         0.64
/* Alias for ADC0 peripheral */
#define VBUS_ADC_IRQ_HANDLER                ADC1_IRQHandler
#define VBUS_ADC_IRQ                        ADC1_IRQn
#define SE_12BIT                            4096.0
#define VREF_BRD                            3.300               /* ADC VREF voltage */
#define ADC_THRSHLD                         750

void VBUS_ADC_IRQ_HANDLER(void)
{
	uint32_t g_Adc16ConversionValue = 0;
	static bool low_voltage = false;
	g_Adc16ConversionValue = ADC16_GetChannelConversionValue(VBUS_ADC, 0);
	if (g_Adc16ConversionValue < ADC_THRSHLD && !low_voltage)
	{
		low_voltage = true;
	}
	else if (g_Adc16ConversionValue >= ADC_THRSHLD)
	{
		low_voltage = false;
	}
#if defined __CORTEX_M && (__CORTEX_M == 4U)
    __DSB();
#endif
}
void VBUS_ADC_init(void)
{
    NVIC_SetPriority(VBUS_ADC_IRQ, 4);
    /* Enable ADC1 IRQ */
    EnableIRQ(VBUS_ADC_IRQ);
	 adc16_config_t ADC16_config            = {
	    .referenceVoltageSource     = kADC16_ReferenceVoltageSourceVref,
	    .clockSource                = kADC16_ClockSourceAsynchronousClock, /* ADC clock freq is (5.2Mhz / 8). see ADC electrical characteristics */
	    /* calculated time of conversion is 3.8us. Refer pg 881 of RM */
	    .enableAsynchronousClock    = true,
	    .clockDivider               = kADC16_ClockDivider8,
	    .resolution                 = kADC16_ResolutionSE12Bit,
	    .longSampleMode             = kADC16_LongSampleDisabled,
	    .enableHighSpeed            = false,
	    .enableLowPower             = false,
	    .enableContinuousConversion = true};

    adc16_hardware_compare_config_t compare_config = { .hardwareCompareMode = kADC16_HardwareCompareMode0,
        .value1 = (int) (VBUS_THRESH * SE_12BIT / VREF_BRD)
    };

    /* Initialize ADC16 converter */
    ADC16_Init(VBUS_ADC, &ADC16_config);
    ADC16_EnableHardwareTrigger(VBUS_ADC, false);
    /* Setting hardware compare value */
    ADC16_SetHardwareAverage(VBUS_ADC, kADC16_HardwareAverageCount8);

    /* Auto-calibrate the ADC value */
    ADC16_DoAutoCalibration(VBUS_ADC);
    ADC16_SetHardwareCompareConfig(VBUS_ADC, &compare_config);
    /* Set channel and enable generation of interrupt */
    ADC16_SetChannelConfig(VBUS_ADC, 0, &VBUS_ADC_channelsConfig);
    //ADC16_SetHardwareAverage(VBUS_ADC, kADC16_HardwareAverageCount32);
    return;
}

 

 

Here, I am not able to get interrupt when ADC voltage is < value1.

0 Kudos
Reply
5 Replies

2,442 Views
diego_charles
NXP TechSupport
NXP TechSupport

 

Hi  

If the ADC interrupt was not triggered it is possible the last ADC conversion was above your threshold value.

You could try to comment the ADC16_SetHardwareCompareConfig call in your code and check if the ADC interrupt is triggered as expected.

I tested on my FDRM-K64F, using the ADC0, after modifying the interrupt example to have a continuous conversion, and adding a threshold value of 1000, I was able to enter to the interrupt when the ADC conversion was below the threshold.

If required I can share my configurations , but they almost similar to yours.  In my case I called the ADC16_SetHardwareCompareConfig after initializing the ADC and setting the ADC trigger to false.

I am curious regarding your custom board configuration. I assume that you can read properly the ADC even using a pulling example, right?

Regards, Diego

 

0 Kudos
Reply

2,422 Views
darshan_shah1
Contributor II

Hi,

Sorry one of my configuration is missing in the post that is as below,

adc16_channel_config_t VBUS_ADC_channelsConfig = {
    .channelNumber = 16U,
    .enableDifferentialConversion = false,
    .enableInterruptOnConversionCompleted = false};

So I would like to get interrupt only when ADC converted value is less than value1 as per  compare_config.

I would not like to get interrupt on every conversion.

0 Kudos
Reply

2,410 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @darshan_shah1 

Thank you for your reply

Could you try to change the:

enableInterruptOnConversionCompleted = false

to
enableInterruptOnConversionCompleted = true. 

it seems that you will need to enable the channel interrupt also.

Regards,

Diego

0 Kudos
Reply

2,394 Views
darshan_shah1
Contributor II

Hi,

With the suggested change I am able to get interrupt. Thank you.

In my system once voltage goes down, it will never comes up and so I am getting interrupt continuously.

Is there any provision to get interrupt only one time?

0 Kudos
Reply

2,359 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @darshan_shah1 

Since in your configuration you had a continuous conversion mode enabled for the ADC. The ADC interrupts will be triggered periodically when the conversion falls into the compare range. I am afraid that there is no provision to have only one interrupt with that setting.


In this case, you will need to analyze how often the signal you are checking changes in your system. If the signal changes very slowly, (compared to ADC sample rate or anything else in your system ) I am thinking that you may disable the ADC interrupts after one was triggered, then enable the ADC interrupts again in a certain time . Or configure the ADC in a non-continuous conversion mode, then trigger a single conversion every once in a while , if the signals is in the compare range, the ADC will trigger a single interrupt.

My apologies for the delayed reply,

Regards, 

Diego.

0 Kudos
Reply