JN-AN1247 compile error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN-AN1247 compile error

ソリューションへジャンプ
504件の閲覧回数
yanggx98
Contributor II

Hi,All

These days I've been trying to modify part of the code for 1247. I followed the standard procedure to import 1247 into my IDE, modified the IDE path, adjusted the SDK path, and changed the chip model. However, I encountered the following errors. The SDK version I'm using is 2.6.13, the IDE version is 11.7.1, and the 1247 version is the latest—all as specified in the documentation.

 

 

 

10:50:02 **** Incremental Build of configuration ControlBridge_Full_GpProxy_1000000 for project JN-AN-1247-Zigbee-3-0-IoT-Control-Bridge ****
make TRACE=1 NODE=FULL_FUNC_DEVICE GP_SUPPORT=1 BAUD=1000000 -r all
Building Node Full functionality ...
"NOTE: Make sure that app_GP.cfg Manually Changed to have device ID as 0x0061 and also remove GP cluster id from in cluster list of Endpoint 242 for Proxy build"
Creating folders...


Building trace version ...
JENNIC_MAC is Mini MAC shim
JENNIC_MAC_PLATFORM is SOC
rm -f ../../Source/ControlBridge/pdum_gen.* ../../Source/ControlBridge/zps_gen*.* ../../Source/ControlBridge/pdum_apdu.*
Compiling C:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZigbeeCommon/Source/port_JN518x.c into ../../Binaries/ControlBridge_Full_GpProxy_1000000/obj/port_JN518x.o ...
C:/yanggx/Programs/NXP/MCUXpressoIDE_11.7.1_9221/ide/tools/bin/arm-none-eabi-gcc -c -o ../../Binaries/ControlBridge_Full_GpProxy_1000000/obj/port_JN518x.o -DgClkUseFro32K=1 -DgPWR_UseAlgoTimeBaseDriftCompensate=1 -DgClkRecalFro32K=0 -DAPP_LOW_POWER_API -DUART_BAUD_RATE=1000000 -DFULL_FUNC_DEVICE -DCRC_XOR -DJENNIC_DEBUG_ENABLE -DGP_PROXY_BASIC_DEVICE -DGP_CERITIFICATION_TEST -DCLD_GREENPOWER -DJN518x=5189 -DJN5189=5189 -DJENNIC_CHIP_NAME=_JN5189 -DJENNIC_CHIP_FAMILY_NAME=_JN518x -D__JN518X__ -DCPU_JN518X -std=gnu99 -DCORE_M4 -D__CODE_RED -fno-common -fmessage-length=0 -fno-builtin -mcpu=cortex-m4 -mthumb -fomit-frame-pointer -Os -fshort-enums -Wall -Wpacked -fdata-sections -ffunction-sections -DWATCHDOG_ALLOWED -fno-lto -DLITTLE_ENDIAN_PROCESSOR -DJENNIC_HW_BBC_RXINCCA=1 -DJENNIC_HW_BBC_DMA=1 -DJENNIC_HW_BBC_ISA=0 -DJENNIC_SW_EXTERNAL_FLASH=0 -DUART_BACKWARDS_COMPATIBLE_API=1 -DRXPOWERADJUST_SUPPORT -I../board -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/CMSIS/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/boards/jn5189dk6 -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/boards/jn5189dk6 -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/components/serial_manager -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/components/uart -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/devices -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/devices/JN5189 -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/devices/JN5189/drivers -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/devices/JN5189/utilities/debug_console -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/devices/JN5189/utilities/str -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/Common -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/ieee-802.15.4/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/ieee-802.15.4/uMac/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/ieee-802.15.4/mMac/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/XCVR/DK6 -DJENNIC_CHIP=JN5189 -DJENNIC_CHIP_JN5189 -DJENNIC_CHIP_FAMILY=JN518x -DJENNIC_CHIP_FAMILY_JN518x -DJENNIC_STACK_MAC -DJENNIC_MAC_MiniMacShim -Wall -Wunreachable-code -DEMBEDDED -DosNumberOfSemaphores=0 -DosNumberOfMutexes=0 -DosNumberOfMessageQs=0 -DosNumberOfMessages=0 -DosNumberOfEvents=5 -DgMainThreadStackSize_c=0 -DgMainThreadPriority_c=7 -DgTaskMultipleInstancesManagement_c=0 -DFSL_OSA_BM_TIMER_CONFIG=FSL_OSA_BM_TIMER_SYSTICK -DgFlashEraseDuringWrite=0 -DgInvalidateHeaderLength=336 -DgEepromType_d=gEepromDevice_InternalFlash_c -DgOtaVerifyWrite_d=0 -DgBootData_None_c=1 -DgEePromParams_BufferSize_c=512 -DgEepromParams_bufferedWrite_c=1 -DgEepromParams_CurrentOffset=0 -DDBG_ENABLE -DDEBUG_ENABLE -DENABLE_RAM_VECTOR_TABLE -DSDK_DEVICE_FAMILY=JN5189 -DgPWRM_Support=1 -DgSupportBle=0 -DcPWR_FullPowerDownMode=1 -DZIGBEE_USE_FRAMEWORK=1 -DPDM_USER_SUPPLIED_ID -DPDM_NO_RTOS -DZPS_APL_OPT_SINGLE_INSTANCE -DOTA_NO_CERTIFICATE -DPLME_SAP -DZBPRO_DEVICE_TYPE_ZCR -DBDB_SUPPORT_NWK_STEERING -DBDB_SUPPORT_NWK_FORMATION -DBDB_SUPPORT_TOUCHLINK -DBDB_SUPPORT_OOBC -I../../Source/ControlBridge -I../../Source/Common -I../../Source/board_k32w0 -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/SerialMAC/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZPSMAC/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZPSNWK/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZPSTSV/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZigbeeCommon/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZPSAPL/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/PWRM/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/PDUM/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/Lists -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/PDM/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/DBG/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/boards/jn5189dk6 -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/devices/JN5189 -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/DebugExceptionHandlers_jn518x/src/../inc -I/../Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/DebugFifo/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/OSAbstraction/Interface -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/FunctionLib -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/SecLib -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/RNG/Interface -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/MemManager/Interface -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/Panic/Interface -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/Messaging/Interface -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/OtaSupport/Source/../Interface/ -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/TimersManager/Interface/ -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/Flash/Internal -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/Flash/External/Source/../Interface/ -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/Flash/Internal/../Interface/ -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/Panic/Interface/ -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/devices/JN5189/drivers -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/components/serial_manager/ -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/components/uart -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/platform -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/LowPower/Source/jn5189dk6/../../Interface/jn5189dk6 -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/framework/GPIO -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCIF/Source -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCIF/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Source -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/MeasurementAndSensing/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Lighting/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/HVAC/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Closures/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SecurityAndSafety/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SmartEnergy/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/OTA/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Commissioning/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/ApplianceManagement/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/GreenPower/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/Generic/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZLO/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/HVAC/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/Closures/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/SecurityAndSafety/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/SmartEnergy/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/ApplianceManagement/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZGP/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/BDB/Include -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/BDB/Source/Common -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/BDB/Source/NwkSteering -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/BDB/Source/NwkFormation -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/BDB/Source/TouchLink -IC:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/BDB/Source/OutOfBand C:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/ZigbeeCommon/Source/port_JN518x.c -MD -MF ../../Binaries/ControlBridge_Full_GpProxy_1000000/obj/.d -MP

Configuring the PDUM ...
C:/yanggx/Programs/NXP/SDKPackages/SDK_2_6_13_JN5189DK6/middleware/wireless/zigbee/tools/PDUMConfig/Source/PDUMConfig -z ControlBridge -e LITTLE_ENDIAN_PROCESSOR -f ../../Source/ControlBridge/ControlBridge_Full_GpProxy.zpscfg -o ../../Source/ControlBridge
make: *** [Makefile:545: ../../Source/ControlBridge/pdum_gen.c] Error 49
"make TRACE=1 NODE=FULL_FUNC_DEVICE GP_SUPPORT=1 BAUD=1000000 -r all" terminated with exit code 2. Build might be incomplete.

10:50:07 Build Failed. 1 errors, 0 warnings. (took 5s.18ms)

 

0 件の賞賛
返信
1 解決策
472件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello,

 

This error may be due to some missing python modules, could you please try installing lxml module for python using python version 3.10.4 or higher? You can try using in python:

pip install lxml

 

Also, please consider upgrading pip.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
473件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello,

 

This error may be due to some missing python modules, could you please try installing lxml module for python using python version 3.10.4 or higher? You can try using in python:

pip install lxml

 

Also, please consider upgrading pip.

0 件の賞賛
返信
449件の閲覧回数
yanggx98
Contributor II
Thank you for your reply. Do you mean that it requires me to have a Python environment on Windows?
0 件の賞賛
返信