Is there any non-blocking function for QN9080?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any non-blocking function for QN9080?

1,038件の閲覧回数
ashkanrezaee
Contributor III

I'm using QN9080 DK connected to a computer via USB port(UART), and I have a while loop which is necessary to work in this loop until user press any key on the keyboard. Is there any non-blocking function for this? (I need an unblocking function such as "kbhit") or something that can reset the microcontroller.

ラベル(1)
0 件の賞賛
返信
1 返信

973件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

What do you mean by reset the MCU ?

Could you please check the following examples ?

qn908xcdk_usb_examples_usb_device_cdc_vcom_freertos

qn908xcdk_usb_examples_usb_device_composite_hid_mouse_hid_keyboard_freertos

Regards,

Estephania

0 件の賞賛
返信