Hi Tyler Wong,
About set the pin on a certain pin to trigger the IRQ, you need to check the pins which has the IRQ function, then use this code to select the IRQ pin:
PORT_SetPinSelect(kPORT_IRQ, kPORT_IRQ_PTA5); /* pin 79 is configured as IRQ *
You can find the KE06 IRQ pin is:
kPORT_IRQ_PTA5 = 0U, /*!< IRQ is mapped to PTA5. */
kPORT_IRQ_PTI0 = 1U, /*!< IRQ is mapped to PTI0. */
kPORT_IRQ_PTI1 = 2U, /*!< IRQ is mapped to PTI1. */
kPORT_IRQ_PTI2 = 3U, /*!< IRQ is mapped to PTI2. */
kPORT_IRQ_PTI3 = 4U, /*!< IRQ is mapped to PTI3. */
kPORT_IRQ_PTI4 = 5U, /*!< IRQ is mapped to PTI4. */
kPORT_IRQ_PTI5 = 6U, /*!< IRQ is mapped to PTI5. */
kPORT_IRQ_PTI6 = 7U, /*!< IRQ is mapped to PTI6. *
So, unfortunately, your PTC0 pin don't have the IRQ function, you also can find the details from the KE06 reference manual, chapter 10.2.1 Signal multiplexing and pin assignments.

Do you mind to use the other IRQ pin, or just need to use the PTC0?
If you want to use PTC0, you also can use it's KBI function, then use the KBI interrupt to detect it.
About the KBI code, you can refer to the SDK examples which located in this folder:
SDK_2.6.0_FRDM-KE06Z\boards\frdmke06z\driver_examples\kbi
Wish it helps you!
If you still have questions about it, please kindly let me know.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------