How can I implement Ethernet with LPC4370?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I implement Ethernet with LPC4370?

1,959 次查看
p_bersch
Contributor I

I am working with the MCUXpresso IDE, developing a device with LPC4370FET100 MCU. Now I want to add Ethernet functionality (TCP, MQTT...).
I understand that I can get the Ethernet stack as middleware library. I built and downloaded some SDK; since I couldn't build the SDK for the LPC4370, I did it for the LPC54018. I installed the SDK and imported the lwip examples. What do I have to do to adapt this examples for the LPC4370 controller?

0 项奖励
回复
5 回复数

1,815 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Patricia Bersch

MCUXpresso SDK doesn't support LPC4370. For this part, we use LPCOpen instead.

Please download LPCOpen for LPC4370 from here:

LPCOpen Software for LPC43XX | NXP 

some lwip demos are included.

Best Regards

Jun Zhang

0 项奖励
回复

1,815 次查看
p_bersch
Contributor I

Hi Jun Zhang,

I had downloaded lpcopen_3_02_lpcxpresso_link2_4370 before (and did it again). But I couldn't find any lwip examples.

I also downloaded lpcopen_3_02_keil_iar_lpclink2_4370; within this ZIP file I can see a lwip folder, and within the folder /LPC43xx_18xx/examples_43xx_18xx/ there are some lwip-Examples. But I can't import these projects into MCUXpresso - I guess because they are built for the Keil / Iar toolchain.

Best Regards

Patricia

0 项奖励
回复

1,815 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, we don't have exact lwip LPC4370 for MCUXpresso IDE, user need import it from IAR/Keil themselves.

Or 

refer lpcopen for LPC4337 , it includes MCUXpresso IDE lwip demo code.

0 项奖励
回复

1,815 次查看
p_bersch
Contributor I

The LPCOpen  v3.02 (Release Date 12/21/2017), which applies to NXP LPCXpresso4337 as well as to LPC-Link 2 (LPC4370) board, doesn't contain the lwip library or any lwip examples any more.

As Legacy download I found LPCOpen v2.20 (Release Date: 10/24/2016), which contains MCUXpresso IDE lwip Examples for the 4337. Hopefully I can convert it for the 4370...

0 项奖励
回复

1,815 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, LPCOpen for LPC4337 v2.2 includes the lwip demo 

0 项奖励
回复