Firmware Upload using LPC LINK-2 possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware Upload using LPC LINK-2 possible?

Jump to solution
4,308 Views
hemanthvasista
Contributor IV

Hello ,

Is it possible to get firmware (xxx.axf) of the connected target (upload)?

I am having LPC LINK-2 in MCUXPRESSO IDE.

regards,

Hemanth

Labels (1)
1 Solution
4,160 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Hemanth,

Do you want to read back firmware from target chip? You can only read back binary firmware. It's impossible to read  back .axf file. https://www.programmersought.com/article/3980249048/ 

MCUXpresso can't read data back. You can download jlink application to LPC LINK2 and use Segger software to read.  

pastedImage_2.png

Regards,

Jing

View solution in original post

6 Replies
4,160 Views
andybeeson
NXP Employee
NXP Employee

As you are already using MCUXpresso IDE, you could alternatively just use the IDE's Memory View - which will work with any supported debug probe - including the LPC-Link2 with the default NXP CMSIS-DAP firmware.  More details in this previous post : https://community.nxp.com/message/997053?commentID=997053#comment-996621 

Hope this helps!

4,160 Views
hemanthvasista
Contributor IV

Hello Andy,

Thanks for your valuable inputs, its easier as my development IDE is MCUxpresso.

regards,

Hemanth

0 Kudos
Reply
4,161 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Hemanth,

Do you want to read back firmware from target chip? You can only read back binary firmware. It's impossible to read  back .axf file. https://www.programmersought.com/article/3980249048/ 

MCUXpresso can't read data back. You can download jlink application to LPC LINK2 and use Segger software to read.  

pastedImage_2.png

Regards,

Jing

4,160 Views
hemanthvasista
Contributor IV

Hello Jing,

Thanks!! I was looking for a similar tool.

Do I need a J-Link license to use this?

I tried enumerate the LPC LINK-2 as J-Link, but it is unable to connect by USB.

I referred to below link:

https://www.segger.com/products/debug-probes/j-link/models/other-j-links/lpc-link-2/ 

Could you help me enumerate LINK-2 as J-Link?

Thanks!!

regards,

Hemanth

0 Kudos
Reply
4,160 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Please use this tool.

LPCScrypt v2.1.1 | NXP 

Regards,

Jing

0 Kudos
Reply
4,160 Views
hemanthvasista
Contributor IV

Hello Jing,

Thanks for your inputs. It worked for me now.

The problem, I forgot to put back the JP1 in LPC LINK-2.

Thanks for your inputs!!

regards,

Hemanth

0 Kudos
Reply