FLEXIO_CAMERA_Init

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLEXIO_CAMERA_Init

1,980 Views
1104883515
Contributor I

请问这个函数是在哪个文件里?

这个文件那里可以下载到。

which file includes this function?

where can I get this file?

I really need this lib, please, thank you!

0 Kudos
Reply
3 Replies

1,858 Views
1104883515
Contributor I

RT1052, can you tell me where I can get these libs(fsl_flexio_camera, fsl_flexio_camera_adapter,fsl_flexio_camera_edma  )

0 Kudos
Reply

1,858 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

Let me check this issue and will update you later

Regards

Daniel

0 Kudos
Reply

1,857 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Wenda:

The flexio interface is for Kinetis parts. Not sure this example has ported to i.mx RT .

The i.MX RT1050 processor has the special camera sensor interface (CSI) module, especially meant for parallel camera connection. So, there is no need of using FlexIO modules.

For the example of the CSI module use, please refer to the AN12110 Application note and the corresponding example, available on below link

https://www.nxp.com/docs/en/application-note/AN12110.pdf 

pastedImage_2.png

0 Kudos
Reply