FLEXIO_CAMERA_Init

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FLEXIO_CAMERA_Init

1,962件の閲覧回数
1104883515
Contributor I

请问这个函数是在哪个文件里?

这个文件那里可以下载到。

which file includes this function?

where can I get this file?

I really need this lib, please, thank you!

0 件の賞賛
返信
3 返答(返信)

1,840件の閲覧回数
1104883515
Contributor I

RT1052, can you tell me where I can get these libs(fsl_flexio_camera, fsl_flexio_camera_adapter,fsl_flexio_camera_edma  )

0 件の賞賛
返信

1,840件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

Let me check this issue and will update you later

Regards

Daniel

0 件の賞賛
返信

1,839件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Wenda:

The flexio interface is for Kinetis parts. Not sure this example has ported to i.mx RT .

The i.MX RT1050 processor has the special camera sensor interface (CSI) module, especially meant for parallel camera connection. So, there is no need of using FlexIO modules.

For the example of the CSI module use, please refer to the AN12110 Application note and the corresponding example, available on below link

https://www.nxp.com/docs/en/application-note/AN12110.pdf 

pastedImage_2.png

0 件の賞賛
返信