Does 1189 SDK support using ENETC 0 and ENETC 1 simultaneously?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does 1189 SDK support using ENETC 0 and ENETC 1 simultaneously?

607件の閲覧回数
arunkumar_g
Contributor IV

Hello,

I have a need to use ENETC 0 and 1 simultaneously, ie two lwip interfaces, where ENETC1 interface communicates with general ethernet while ENETC0 interface communicates with another cpu. Currently I find only one NETC can we used (via define NETC_PSI).

I also find that even though ethernetif1_init is defined in header, it is never implemented in SDK.

Note: RT1189 EVK/FreeRTOS/lwip/SDK v2.16.

Thanks

 

 

0 件の賞賛
返信
1 返信

587件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @arunkumar_g,

Since the RT1180 is still in preproduction and therefore not yet public, we are not able to provide you with information about this product on the public community forum just yet. Please contact your NXP representative that provided you with this device for the latest information about the simultaneous use of ENETC 0 and ENETC 1 on the RT1180.

Sorry for the inconvenience and thank you for your understanding.

BR,
Edwin.

0 件の賞賛
返信