Compile Error with SDK Example Code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Compile Error with SDK Example Code

跳至解决方案
3,939 次查看
duglew60
Contributor II

I'm using the gnu toolchain, arm-gnu-toolchain-13.2.Rel1-x86_64-arm-none-eabi, on WSL2 Ubuntu to compile the example code that is with the SDK_2_9_0_MEK-MIMX8QX.  The specific code I'm trying to build is rpmsg_lite_str_echo_rtos and I've also tried the hello world example.  I'm using the build_debug.sh script.  I'm getting the following error:

MIMX8QX6/utilities/fsl_sbrk.c:22:1: error: unknown type name 'caddr_t'

From the research I've done this is related to BSD-ism in older code.  Is there an environment variable I can set to correct this error?  My research is saying I need to modify the code but I would figure NXP would make code available that does build without basic code modifications.

 

0 项奖励
回复
1 解答
3,917 次查看
duglew60
Contributor II

Following your instructions the hello_world demo program built successfully:

[ 92%] Building C object CMakeFiles/hello_world.elf.dir/home/dlewis/nxp-projects/SDK_2_9_0_MEK-MIMX8QX/devices/MIMX8QX6/drivers/fsl_gpio.c.obj
[ 96%] Building C object CMakeFiles/hello_world.elf.dir/home/dlewis/nxp-projects/SDK_2_9_0_MEK-MIMX8QX/devices/MIMX8QX6/utilities/fsl_sbrk.c.obj
[100%] Linking C executable release/hello_world.elf
[100%] Built target hello_world.elf

 

 

在原帖中查看解决方案

3 回复数
3,887 次查看
duglew60
Contributor II

Thank you for your help Alejandro.

3,923 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @duglew60 

 

I hope you are doing well.

Could you please try:

Download gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 from https://developer.arm.com/downloads/-/gnu-rm

Then:

$ tar -xf gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 
$ export ARMGCC_DIR=~/gcc-arm-none-eabi-10.3-2021.10
$ export PATH=$PATH:~/gcc-arm-none-eabi-10.3-2021.10

 

Go to SDK example directory (In my case):

$cd ~/SDK_2_9_0_MEK-MIMX8QX.tar/SDK_2_9_0_MEK-MIMX8QX/boards/mekmimx8qx/demo_apps/hello_world/armgcc

 

And please run the build_release.sh

$./build_release.sh

 

Please let me know how it was.

 

Best regards!

0 项奖励
回复
3,918 次查看
duglew60
Contributor II

Following your instructions the hello_world demo program built successfully:

[ 92%] Building C object CMakeFiles/hello_world.elf.dir/home/dlewis/nxp-projects/SDK_2_9_0_MEK-MIMX8QX/devices/MIMX8QX6/drivers/fsl_gpio.c.obj
[ 96%] Building C object CMakeFiles/hello_world.elf.dir/home/dlewis/nxp-projects/SDK_2_9_0_MEK-MIMX8QX/devices/MIMX8QX6/utilities/fsl_sbrk.c.obj
[100%] Linking C executable release/hello_world.elf
[100%] Built target hello_world.elf