Hi,
Let's take a look at https://github.com/Masmiseim36/nxpSDK samples.
The problem I want to discuss exists across many samples. Let's take evkmimxrt1010/usb_examples/usb_device_composite_hid_audio_unified/bm for specificity.
USB_DeviceHidKeyboardAction() is regularly called from the main() cycle.
It calls USB_DeviceHidSend() function, which accesses interruptInPipeBusy, interruptInPipeStall, interruptInPipeDataBuffer fields.
And the same fields can be accessed from under USB IRQ handler (during kUSB_DeviceClassEventClearEndpointHalt, etc operations).
Which can lead to unintended effects.
How can we get protection from this?
Would it be a good idea to disable USB interrupts in USB_DeviceHidKeyboardAction() function before calling USB_DeviceHidSend() and enable them afterwards? Will there be any problems because deep within USB_DeviceHidSend() function there are DisableGlobalIRQ + EnableGlobalIRQ operations being performed?
解決済! 解決策の投稿を見る。
Hi @olex,
Thanks for the explanation, I understand.
I hypothesize that your modification would be useful for the mentioned cases where a USB ISR can occur during main() execution.
I don't think it will cause any unwanted behavior but rather will add robustness to the application.
Hi @olex,
Thank you for the clarifications. I highly recommend you use the official NXP SDK repository as a base for the USB driver on our devices, especially if the issue you mention with the interruptInPipeStall and interruptInPipeDataBuffer fields is not present in it.
It's still good to have this post describe the possibility of the problem you mention in case someone in the future stumbles upon the same situation as you did.
Thanks for reporting this.
BR,
Edwin.
Hi @olex,
Firstly, the oficial distribution of NXP's SDK is via the following GitHub repository: GitHub - nxp-mcuxpresso/mcuxsdk-manifests: Manifest repo for MCUXpresso SDK project
Or the following SDK builder page: Select Board | MCUXpresso SDK Builder
Secondly, I'm not quite sure I understand why the access of interruptInPipeBusy, interruptInPipeStall, interruptInPipeDataBuffer fields on the USB_DeviceHidSend() function as well as the USB IRQ handler would lead uninteded consequences.
Could you please elaborate on this?
BR,
Edwin.
Hi Edwin,
I have updated information.
SDK version 25.06. Downloaded via MCUXpresso IDE v25.6 or directly from SDK Builder web-site.
Let's take EVK-MIMXRT1010 board, usb_device_composite_hid_audio_unified_bm example.
Official SDK also has an issue with interruptInPipeStall field and similar ones, which I described earlier.
Therefore, my question still stands.
Would it be a good idea to call DisableIRQ( UsbIrqNumber ) in USB_DeviceHidKeyboardAction() function before calling USB_DeviceHidSend() and enable it afterwards? Will there be any problems because deep within USB_DeviceHidSend() function there are DisableGlobalIRQ + EnableGlobalIRQ operations being performed?
Hi @olex,
Thanks for the update.
Normally we wouldn't recommend changing the device drivers like that. Could you describe a situation where the problem you describe might appear? I'm not completely sure I understand where the issue lies on the USB drivers.
Thanks for the clarifications.
Hi Edwin,
Below is an excerpt from USB_DeviceHidSend() function implementation:
main() cycle periodically calls USB_DeviceHidSend()
and USB ISR also calls USB_DeviceHidSend() periodically
USB ISR can occur/intervene at any arbitrary point in main() execution, including the point between checking busy-flag and setting it to 1.
As a result, we will get an inconsistent "parallel" code execution.
And SDK middleware has many functions similar to USB_DeviceHidSend() described. The same applies to example applications.
My proposal is not to change the drivers code, but to change the way the driver functions are used in the application.
I want to disable USB interrupts during USB_DeviceHidSend() is called from the context of main().
Is this a normal idea?
Hi @olex,
Thanks for the explanation, I understand.
I hypothesize that your modification would be useful for the mentioned cases where a USB ISR can occur during main() execution.
I don't think it will cause any unwanted behavior but rather will add robustness to the application.
Thank you, Edwin!
Hi Edwin,
First of all, I would like to apologize for indicating an unofficial repository. When I was just getting started with NXP-chips, a friend recommended setting up MCUXpresso IDE exactly with it. I had no idea it was an unofficial repository:(
In the official repository I don't see interruptInPipeStall and interruptInPipeDataBuffer fields, in the use of which I noticed a problem. So, I don't know if it makes sense to continue the discussion:)
The following code is executed in the main() context:
usb_status_t USB_DeviceHidSend( class_handle_t handle, uint8_t ep, uint8_t* buffer, uint32_t length )
{
usb_device_hid_struct_t* hidHandle;
usb_status_t error = kStatus_USB_Error;
if ( NULL == handle )
return kStatus_USB_InvalidHandle;
hidHandle = (usb_device_hid_struct_t*)handle;
if ( 0U != hidHandle->interruptInPipeBusy )
return kStatus_USB_Busy;
hidHandle->interruptInPipeBusy = 1U;
if ( 0U != hidHandle->interruptInPipeStall )
{
hidHandle->interruptInPipeDataBuffer = buffer;
hidHandle->interruptInPipeDataLen = length;
return kStatus_USB_Success;
}
error = USB_DeviceSendRequest( hidHandle->handle, ep, buffer, length );
if ( kStatus_USB_Success != error )
hidHandle->interruptInPipeBusy = 0U;
return error;
}
And the following code is executed under USB-ISR:
case kUSB_DeviceClassEventSetEndpointHalt:
if ( ( NULL == hidHandle->configStruct ) || ( NULL == hidHandle->interfaceHandle ) )
break;
/* Get the endpoint address */
temp8 = ( (uint8_t*)param );
for ( count = 0U; count < hidHandle->interfaceHandle->endpointList.count; count++ )
{
if ( *temp8 == hidHandle->interfaceHandle->endpointList.endpoint[count].endpointAddress )
{
/* Only stall the endpoint belongs to the class */
if ( USB_IN == ( ( hidHandle->interfaceHandle->endpointList.endpoint[count].endpointAddress & USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_MASK ) >> USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_SHIFT ) )
hidHandle->interruptInPipeStall = 1U;
else
hidHandle->interruptOutPipeStall = 1U;
error = USB_DeviceStallEndpoint( hidHandle->handle, *temp8 );
}
}
break;
case kUSB_DeviceClassEventClearEndpointHalt:
if ( ( NULL == hidHandle->configStruct ) || ( NULL == hidHandle->interfaceHandle ) )
break;
/* Get the endpoint address */
temp8 = ( (uint8_t*)param );
for ( count = 0U; count < hidHandle->interfaceHandle->endpointList.count; count++ )
{
if ( *temp8 == hidHandle->interfaceHandle->endpointList.endpoint[count].endpointAddress )
{
/* Only un-stall the endpoint belongs to the class */
error = USB_DeviceUnstallEndpoint( hidHandle->handle, *temp8 );
if ( USB_IN == ( ( ( *temp8 ) & USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_MASK ) >>
USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_SHIFT ) )
{
if ( 0U != hidHandle->interruptInPipeStall )
{
hidHandle->interruptInPipeStall = 0U;
if ( (uint8_t*)USB_INVALID_TRANSFER_BUFFER != hidHandle->interruptInPipeDataBuffer )
{
error = USB_DeviceSendRequest( hidHandle->handle, ( hidHandle->interfaceHandle->endpointList.endpoint[count].endpointAddress & USB_DESCRIPTOR_ENDPOINT_ADDRESS_NUMBER_MASK ), hidHandle->interruptInPipeDataBuffer, hidHandle->interruptInPipeDataLen );
if ( kStatus_USB_Success != error )
{
usb_device_endpoint_callback_message_struct_t endpointCallbackMessage;
endpointCallbackMessage.buffer = hidHandle->interruptInPipeDataBuffer;
endpointCallbackMessage.length = hidHandle->interruptInPipeDataLen;
endpointCallbackMessage.isSetup = 0U;
USB_DeviceHidInterruptIn( hidHandle->handle, (void*)&endpointCallbackMessage, handle );
}
hidHandle->interruptInPipeDataBuffer = (uint8_t*)USB_INVALID_TRANSFER_BUFFER;
hidHandle->interruptInPipeDataLen = 0U;
}
}
}
else
{
if ( 0U != hidHandle->interruptOutPipeStall )
{
hidHandle->interruptOutPipeStall = 0U;
if ( (uint8_t*)USB_INVALID_TRANSFER_BUFFER != hidHandle->interruptOutPipeDataBuffer )
{
error = USB_DeviceRecvRequest( hidHandle->handle, ( hidHandle->interfaceHandle->endpointList.endpoint[count].endpointAddress & USB_DESCRIPTOR_ENDPOINT_ADDRESS_NUMBER_MASK ), hidHandle->interruptOutPipeDataBuffer, hidHandle->interruptOutPipeDataLen );
if ( kStatus_USB_Success != error )
{
usb_device_endpoint_callback_message_struct_t endpointCallbackMessage;
endpointCallbackMessage.buffer = hidHandle->interruptOutPipeDataBuffer;
endpointCallbackMessage.length = hidHandle->interruptOutPipeDataLen;
endpointCallbackMessage.isSetup = 0U;
USB_DeviceHidInterruptOut( hidHandle->handle, (void*)&endpointCallbackMessage, handle );
}
hidHandle->interruptOutPipeDataBuffer = (uint8_t*)USB_INVALID_TRANSFER_BUFFER;
hidHandle->interruptOutPipeDataLen = 0U;
}
}
}
}
}
break;
If during main() execution an interrupt is triggered at this point:
, and this interrupt handles kUSB_DeviceClassEventClearEndpointHalt event, then the pointer to a some buffer will be saved in interruptInPipeDataBuffer and interruptInPipeDataLen fields.
And this information will be "hidden/waiting" until the next pair of events kUSB_DeviceClassEventSetEndpointHalt + kUSB_DeviceClassEventClearEndpointHalt. Which will unexpectedly send some content to the host (which at that moment will be in that buffer).
I understand that probability of such event is very low, especially in the case of a keyboard. But a similar operating principle is used in many classes/examples: phdc, com-port, etc. That's why I came up with idea of using a protection in the form of disable+enable USB interrupts inside main().