CMISI interrupt priority

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMISI interrupt priority

1,466 Views
tobias_mrs
Contributor III

Hello I work on a Kinetis MKE18F512 with SDK 2.6 and  now I have problems to understand and use the interrupts in a correct way.
My Problem:

I have interrupt settings at reset state.
I drive a system-timer wit the sysTick interrupt. Now if I use a UART transfer the sysTick don't run and I don't get any timings.
It also don't help to lower the UART interrupt priority by

   NVIC_SetPriority( LPUART0_TX_IRQn, 1 );
   NVIC_SetPriority( LPUART0_RX_IRQn, 1 );
   NVIC_SetPriority( CAN0_ORed_IRQn, 2 );
   NVIC_SetPriority( CAN0_Error_IRQn, 2 );
   NVIC_SetPriority( CAN0_Wake_Up_IRQn, 2 );
   NVIC_SetPriority( CAN0_ORed_Message_buffer_IRQn, 2 );

If one interrupt is running no other will be called.
How could I setup that the systick interrupt can preempt all others?

0 Kudos
Reply
2 Replies

1,354 Views
tobias_mrs
Contributor III

I have found the problem:

The function SysTick_Config(uint32_t ticks) set the interrupt priority of the sysTick to 15. That means the lowest priority.

The solution was to reset the priority after calling the init function

    if( 0 != SysTick_Config( SystemCoreClock / 1000 ) )
    {
        ret = HAL_ERR_INIT;
    }
    else
    {
        NVIC_SetPriority( SysTick_IRQn, 0 );
        // no errors
    }  


Bu for further information's.
Could you lead me to a example how to configure the interrupt priority with the SDK.

0 Kudos
Reply

1,354 Views
nxf58474
NXP Employee
NXP Employee

Hi Tobias,

 

I am very happy that the problem has been resolved. Unfortunately, there are no examples with that specific functionality that show the use of NVIC.

 

If you have any questions please don't hesitate to ask.

 

Best Regards,

Ricardo

0 Kudos
Reply