Bug: tx buffers should be const in fsl_dspi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug: tx buffers should be const in fsl_dspi

1,978 Views
davenadler
Senior Contributor I

Using SDK2.8, MCUXpresso 11.2, Kinetis K64F

Lots of applications (like ours) will send SPI data from const structures (ie flash), so...

tx buffer pointers need to be const (and probably volatile is not required).
Please fix:
fsl_dspi.h (typdef/structs dspi_transfer_t, _dspi_master_handle, _dspi_slave_handle)
fsl_dspi.c (function DSPI_MasterTransferBlocking)

Thanks!
Best Regards, Dave

PS: Fixes attached.

Tags (3)
4 Replies

1,858 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Dave,

But also in many cases, the transmit data is variable, not from flash or const type. Customer can adjust driver due to their application. Driver can't cover all user applications.

Regards,

Jing 

0 Kudos
Reply

1,858 Views
davenadler
Senior Contributor I

nxf32199‌ - Apparently you do not understand "const" here.
"const" means "I will treat this as constant and will not modify it".
It does not mean that the input to the routine must be a constant.
Please confirm you have understood this and filed a bug report.
Thanks,
Best Regards, Dave

0 Kudos
Reply

1,858 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, I understand.

The benefit of this modification is buffer pointer can use on both normal variable type and const type.

The disadvantage is this pointer can't transfer to other function which want to modify the data in this buffer. But this is not a big problem.

So, yes, your suggestion is very good. I'll transmit to software team.

Thanks

Jing 

0 Kudos
Reply

1,858 Views
davenadler
Senior Contributor I

jingp18@yahoo.com‌ - To be very clear, your statement above is absolutely incorrect:
The disadvantage is this pointer can't transfer to other function which want to modify the data in this buffer.

An API for transmitting data should never modify the transmitted data.
Thus any such API should declare a tx input as const.
Just like strcpy declares it's input as const:
Got it?

   char * strcpy ( char * destination, const char * source );

0 Kudos
Reply