Bug in LPSPI_MasterTransferBlocking() if bytesPerFrame < 4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug in LPSPI_MasterTransferBlocking() if bytesPerFrame < 4

2,343件の閲覧回数
kevin_haake
Contributor II

There seems to be an issue in LPSPI_MasterTransferBlocking() (as found in fsl_lpspi.c / SDK 2.7, MKE14F512VLL16). A related issue existed in SDK v2.6. (see Bug in LPSPI_MasterTransferBlocking()?). A fix was put in for SDK release 2.7 to address it, but I believe there is still a problem if bytesPerFrame is less than 4.

What I have observed is that if this function is preempted/interrupted for a substantial length of time at the wrong time, an overrun can still occur in the Rx FIFO which causes the function to get stuck in an endless loop and never return. I believe the problem is that the rxFifoMaxBytes value is initialize improperly for bytesPerFrame values less than 4.


This value is currently set in SDK 2.7 as follows:

uint32_t rxFifoMaxBytes = 4U * fifoSize;

I believe it should instead take bytesPerFrame into consideration. Something like:

uint32_t rxFifoMaxBytes = ((bytesPerFrame <= 4U) ? bytesPerFrame : 4U) * fifoSize;

In my case, I was using a bits per frame setting of 8 (so my bytesPerFrame is 1), and observed the same lockup as before. After putting in the proposed fix, the lockup no longer occurs.

ラベル(1)
1 返信

2,256件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Kevin:

Thanks for sharing your feedback.

There is a bug fix for this issue in SDK 2.8.0_EVKB-IMXRT1050, which will be released later this month.

Regards

Daniel