Hi embeddeddavid,
The following SDK code works OK or not on your side with FRDM-K64 board:
SDK_2.7.0_FRDM-K64F\boards\frdmk64f\lwip_examples\lwip_udpecho
In the previous reply, you told me that the UDP Echo example works alright, but SDK 2.7.0 and lwIP 2.1.2.0 is causing bad UDP communication. So, if totally SDK2.7.0, without the SDK2.6 code, whether has the UDP communication issue on your side now?
I just want to make sure whether the FRDM-K64 with SDK2.7.0 has the UDP communication issue or not, then I can try to reproduce your issue, and check more details.
You also can share the Wireshark test result pictures which demonstrate the bad UDP communication.
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------