Available modes for peripherals configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Available modes for peripherals configuration

4,007 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hi,

We are working with the SDK_2.6.2 version for MIMXRT1062xxxxA processor on a MIMXRT1060-EVK and I have a few questions regarding the available configuration modes for peripherals inside MCUXpresso Config Tools.

For example, each instance of the LPSPI peripheral has 5 user configurable modes (Polling, Interrupts, Transfer, eDMA and FreeRTOS). I have understood from the API Reference Manual that the Polling mode requires the use of the transfer blocking functions, while an Interrupt mode uses a non blocking data transfer.

However, when using a TransferNonBlocking function, the structure named handle, passed as a second parameter to the function, has fields which are configurable inside the Transfer tab only (e.g: Continuous PCS signal or Swap bytes option in case of a Slave instance). If in Interrupt mode, how can I change the default values for these fields inside MCUXpresso Config Tools?

Is the Transfer mode used only for a blocking type of data transfer? If not in Interrupt mode, the generated code in the peripherals.c file does not include the call of the EnableIRQ function.

Could you briefly explain each mode - I'd like to know what use-cases they have.

Thank you in advance,

Irina

标记 (3)
9 回复数

3,152 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Irina,

First of all, sorry for the later reply.

About Interrupt transfer mode, there with a demo named [interrupt_b2b\master] with below path:

 ..\boards\evkmimxrt1060\driver_examples\lpspi\interrupt_b2b\master

It will call below structure to define master configuration, such as:

/*Master config*/
masterConfig.baudRate = TRANSFER_BAUDRATE;
masterConfig.bitsPerFrame = 8;
masterConfig.cpol = kLPSPI_ClockPolarityActiveHigh;
masterConfig.cpha = kLPSPI_ClockPhaseFirstEdge;
masterConfig.direction = kLPSPI_MsbFirst;

masterConfig.pcsToSckDelayInNanoSec = 1000000000 / masterConfig.baudRate;
masterConfig.lastSckToPcsDelayInNanoSec = 1000000000 / masterConfig.baudRate;
masterConfig.betweenTransferDelayInNanoSec = 1000000000 / masterConfig.baudRate;

masterConfig.whichPcs = EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT;
masterConfig.pcsActiveHighOrLow = kLPSPI_PcsActiveLow;

masterConfig.pinCfg = kLPSPI_SdiInSdoOut;
masterConfig.dataOutConfig = kLpspiDataOutRetained;

srcClock_Hz = LPSPI_MASTER_CLK_FREQ;
LPSPI_MasterInit(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterConfig, srcClock_Hz);

As my understanding about Transfer mode, which is a higher level of polling/interrupt/DMA mode.

In fact, Transfer mode still need to call one of  polling/interrupt/DMA mode related transactional API function.

Thanks for the attention.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,152 次查看
constantinrazva
NXP Employee
NXP Employee

Hello Hui_Ma,

I have another question regarding this topic - why can't we use continuous mode on SPI in interrupt mode (only available in transfer mode) ?

pastedImage_1.png

Am I missing something? How can we achieve that functionality with only these settings available?

Thank you in advance for answering to these questions.

Kind regards,

Razvan.

3,152 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I think the LPSPI component Mode setting is correct.

The SDK peripheral drivers has two level functional APIs:

pastedImage_1.png

The Transfer mode using transcational API, which based on LPSPI driver provided 

LPSPI_MasterTransferBlocking() or LPSPI_MasterTransferNonBlocking() API functions.

So, the Continuous SCK available for transfer mode.

While, the interrupt and polling mode, just provide low level function API, customer need to write their required transcational API based low-level driver. So, customer need to enable continuous SCK feature with their transactional API function manually.

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,152 次查看
constantinrazva
NXP Employee
NXP Employee

Hello Hui_Ma,

So you are saying that MCUX with CT does not let you work in interrupt mode and also have all the options available - am I right? Let me explain why I find that curious - as you said, 'transfer mode' is on a higher level API than 'interrupt mode' so, for me at least, it makes more sense to have the same or even more hardware options available as you go lower (although I understand that higher level abstraction can sometimes mean less fine grain control).

Thank you for your answers.

Kind regards,

Razvan.

0 项奖励
回复

3,152 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Razvan,

When you check MCUXpresso CT tool generated code with LPSPI interrupts mode, which using below LPSPI init functinon:

void LPSPI_1_init(void) {
LPSPI_MasterInit(LPSPI_1_PERIPHERAL, &LPSPI_1_config, LPSPI_1_CLOCK_FREQ);
/* Enable interrupt LPSPI1_IRQn request in the NVIC */
EnableIRQ(LPSPI_1_IRQN);
}

It just do the LPSPI initialization and enable LPSPI related IRQ at NVIC.

So, cusotmer also still need to call <fsl_lpspi.c> & <fsl_lpspi.h> driver to realise the data transfer.

Just as [lpspi_interrupt_b2b_master] demo showed, when using MCUXpresso CT generated interrupt mode code,

customer need to call below code to do data transfer:

/*TCR is also shared the FIFO , so wait for TCR written.*/
while (LPSPI_GetTxFifoCount(EXAMPLE_LPSPI_MASTER_BASEADDR) != 0)
{
}
/*Fill up the TX data in FIFO */
while ((LPSPI_GetTxFifoCount(EXAMPLE_LPSPI_MASTER_BASEADDR) < g_masterFifoSize) &&
(masterTxCount - masterRxCount < g_masterFifoSize))
{
/*Write the word to TX register*/
LPSPI_WriteData(EXAMPLE_LPSPI_MASTER_BASEADDR, masterTxData[masterTxCount]);
++masterTxCount;

if (masterTxCount == TRANSFER_SIZE)
{
break;
}
}
LPSPI_EnableInterrupts(EXAMPLE_LPSPI_MASTER_BASEADDR, kLPSPI_RxInterruptEnable);

Daniel had written a document to show how to using [peripheral] component with MCUXpresso CT tool:

https://community.nxp.com/docs/DOC-341986

Wish it helps.

best regards,

Mike

0 项奖励
回复

3,152 次查看
constantinrazva
NXP Employee
NXP Employee

Hello Hui_Ma,

I think you misunderstood me - I am saying that you can use spi interrupt mode, but you don't have access to all settings for it, like enabling continuous mode. I am not sure what you wanted to show with the code snippets or with Daniel Chen's document - which I like, but does not help in clarifying the spi interrupt mode - continuous mode enabling problem.

Kind regards,

Razvan.

0 项奖励
回复

3,152 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Razvan,

Thanks for highlighting the [continuous chip select mode enaaling] option with LPSPI interrupt mode.

I need to check that feature with MCUXpresso CT tool design team.

I will update when there with any feedback. Thanks for the patience.

best regards,

Mike

0 项奖励
回复

3,152 次查看
constantinrazva
NXP Employee
NXP Employee

Hello Mike,

Thank you as well for your support on the matter. I'll wait for the other team's response.

Kind regards,

Razvan.

0 项奖励
回复

3,152 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Razvan,

I forward an email about this topic, you could check the feedback from MCUXpresso Config Tool design team. Thanks.

pastedImage_1.png

best regards,

Mike

0 项奖励
回复