Amazon missing from Amazon FreeRTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Amazon missing from Amazon FreeRTOS

1,832件の閲覧回数
hacksome
Contributor I

Hi

I am working with RT1050 evk. It says in all the marketing that RT1050 SDK comes with "Amazon" freeRTOS. however, all I see is the basic freeRTOS. The other libraries like, wifi, OTA, secure_sockets, crypto, mqtt, that are part and parcel of amazon version,  seem to be missing!

Can you confirm if there is a fully ported version of the Amazon Version of freeRTOS and where can I find it? I did click on the Amazon FreeRtos checkbox when downloading the SDK.

Thanks in advance

0 件の賞賛
返信
1 返信

1,708件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Taimur,

You could refer to the “Getting Started with MCUXpresso SDK and FreeRTOS OS” from SDK documentation package, where is mentioned that MCUXpresso SDK provides FreeRTOS OS version 9.0.0. Detail information about the distribution can befound on www.freertos.org. (see attached document).


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信