processor_version: 9.0.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

processor_version: 9.0.3

ソリューションへジャンプ
3,461件の閲覧回数
GaryYJS
Contributor I

Hello everyone

I have a project where pin_mux.c has the following information.

!!GlobalInfo
product: Pins v9.0
processor: LPC55S16
package_id: LPC55S16JBD100
mcu_data: ksdk2_0
processor_version: 9.0.3
board: LPCXpresso55S16

 

Where can I download this version of the processor?

When I use the latest version of the IDE and use the pin configuration tool it alerts me that the project version is low. Continuing to use the pin configuration tool to generate the source code causes the project to error out.

 

0 件の賞賛
返信
1 解決策
3,450件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello GaryYJS,

processor 9.0.3 means the MCUX Config Tools v9 were used (MCUXpresso IDE from January 2021). Each version of Config Tools has dedicated set of data that might not be compatible with newer/older version of the tools and it is not expected to be combined this way. Either you should download the older Config Tools or try to fix the issue.

Can you share what kind of errors do you see? Compile error or during the run-time?

 

Regards,

Libor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,451件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello GaryYJS,

processor 9.0.3 means the MCUX Config Tools v9 were used (MCUXpresso IDE from January 2021). Each version of Config Tools has dedicated set of data that might not be compatible with newer/older version of the tools and it is not expected to be combined this way. Either you should download the older Config Tools or try to fix the issue.

Can you share what kind of errors do you see? Compile error or during the run-time?

 

Regards,

Libor

0 件の賞賛
返信
3,437件の閲覧回数
GaryYJS
Contributor I

The problem has been solved by using MCUXpressoIDE_11.3.0 which was available on Jan 14, 2021.

Thank you for your help

0 件の賞賛
返信
3,447件の閲覧回数
GaryYJS
Contributor I

Testing directly on the project, everything works fine. When opening the pin configuration tool, a warning appears "The loaded configuration was created by an earlier version of the tool. If you save it, you will not be able to reopen the tool with the old version". Then open an IO port at random, update the source code and do nothing else.
I test again and the error appears, and they are all in resource_config.c

0 件の賞賛
返信