osx install hung

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

osx install hung

2,019 Views
rickledford
Contributor I

log from install:

Apr  5 21:23:59 Rickys-MBP installd[344]: PackageKit: ----- Begin install -----

Apr  5 21:23:59 Rickys-MBP installd[344]: PackageKit: Session UUID file exists - will not overwrite /var/folders/zz/zyxvpxvq6csfxvn_n0000000000000/C/PKInstallSandboxManager/CED4F1E0-B081-4014-84E3-F60C5FE52F17.activeSandbox

I killed the install and looked in Launcher. The IDE is installed and runs. The installer hung without completing installation. What to do?

0 Kudos
Reply
1 Reply

1,899 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Rick,

Could you tell us which OS X version are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply