map file viewer bugs (ASSERT Macro flagged as problem, null-ptr exception)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

map file viewer bugs (ASSERT Macro flagged as problem, null-ptr exception)

ソリューションへジャンプ
4,297件の閲覧回数
davenadler
Senior Contributor II

Viewing a GCC map file in the IDE, ASSERT lines are flagged as a problem:
Description Resource Path Location Type
missing '=' at '(' MFW2.map /MFW2/Debug line: 17202 /MFW2/Debug/MFW2.map Map File Problem


The map file contents are for example:

LOAD ./Generated_uC_setup/pin_mux.o
LOAD C:\git_CAP\repo_MFW2\MFW2\libs\libarm_cortexM4lf_math.a
                0x00016000                HEAP_SIZE = DEFINED (__heap_size__)?__heap_size__:0x400
                0x00000800                STACK_SIZE = DEFINED (__stack_size__)?__stack_size__:0x400
                0x00000001                ASSERT (((HEAP_SIZE & 0xf) == 0x0), HEAP_SIZE must be multiple of 16)
                0x00000001                ASSERT (((STACK_SIZE & 0xf) == 0x0), STACK_SIZE must be multiple of 16)
                0x00016000                _HeapSize = HEAP_SIZE
                0x00000800                _StackSize = STACK_SIZE
                0x00000000                M_VECTOR_RAM_SIZE = 0x0

The link works just fine.

I'm using NXP's MCUXpresso IDE v11.3.0 [Build 5222] [2021-01-11],
which is based on Eclipse CDT 9.11.1.202006011430

Thanks in advance,
Best Regards, Dave

PS: Also... If Eclipse is started with the map file as an open tab, but the map file is not present (for example after a clean), the viewer dies with a null-ptr exception.

PPS: I tried reporting the problem here but got nowhere: https://www.eclipse.org/forums/index.php/m/1852668/#msg_1852668 

0 件の賞賛
返信
1 解決策
4,251件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Thanks for attaching the map file. We're seeing the two warnings on our side as well and logged a ticket to track the issue internally. We'll plan a fix for a future release. Note that the warnings you see during map or linker script parsing are not blocking by any means build or debug.

Regards,

MCUXpresso IDE Support

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,277件の閲覧回数
ErichStyger
Specialist I

Hi @davenadler ,

about the thing of no-existing map file: With 11.5.1 I get nothing unexpected:

ErichStyger_0-1653983406454.png

 

So it could be something which has been fixed meanwhile.

Erich

0 件の賞賛
返信
4,267件の閲覧回数
davenadler
Senior Contributor II

Thanks @ErichStyger as always!
I've attached an example map file to the original post.
Much appreciate the clarification; I assumed the map file viewer was standard Eclipse or CDT...
Thanks,
Best Regards, Dave

0 件の賞賛
返信
4,252件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Thanks for attaching the map file. We're seeing the two warnings on our side as well and logged a ticket to track the issue internally. We'll plan a fix for a future release. Note that the warnings you see during map or linker script parsing are not blocking by any means build or debug.

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信
4,245件の閲覧回数
davenadler
Senior Contributor II

Thanks @ErichStyger and @lpcxpresso_supp !
Best Regards, Dave

0 件の賞賛
返信
4,282件の閲覧回数
ErichStyger
Specialist I

Hi @davenadler ,

this map file parser is a NXP specific feature afik, so the Eclipse community won't act on that. But I'm sure the NXP engineers would like to have a look: I passed a few of such things in the past and they corrected it in the upcoming release.

I tried your snippet with the 11.5.1 version, and that looked ok (warnings, but no assert). Would you be able to share your full map file for a test?

Erich

0 件の賞賛
返信