make (e=87): The parameter is incorrect.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

make (e=87): The parameter is incorrect.

7,046 Views
Emin
Contributor III

I have attached full compile log file. At the end I got this error:

Building target: evklpc55S69_tflm_kws_eiq.axf
Invoking: MCU C++ Linker
arm-none-eabi-c++ -nostdlib -Xlinker -Map="evklpc55S69_tflm_kws_eiq.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -Xlinker --cref -mcpu=cortex-m33 -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -T evklpc55S69_tflm_kws_eiq_Debug.ld -o "evklpc55S69_tflm_kws_eiq.axf" ./utilities/fsl_assert.o ./utilities/fsl_debug_console.o ./utilities/fsl_str.o ./startup/boot_multicore_slave.o ./startup/startup_lpc55s69_cm33_core0.o ./source/model/get_top_n.o ./source/model/model.o ./source/model/model_ds_cnn_ops_micro.o ./source/model/output_postproc.o ./source/audio/audio_capture.o ./source/audio/kws_mfcc.o ./source/audio/mfcc.o ./source/cpp_config.o ./source/demo_info.o ./source/evklpc55S69_tflm_kws_eiq.o ./source/main.o ./source/semihost_hardfault.o ./source/timer.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/SoftmaxFunctions/arm_nn_softmax_common_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q15.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q7.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_s8_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_u8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_with_batch_q7.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/SVDFunctions/arm_svdf_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/SVDFunctions/arm_svdf_state_s16_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ReshapeFunctions/arm_reshape_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/PoolingFunctions/arm_avgpool_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/PoolingFunctions/arm_avgpool_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/PoolingFunctions/arm_max_pool_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/PoolingFunctions/arm_max_pool_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/PoolingFunctions/arm_pool_q7_HWC.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_accumulate_q7_to_q15.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_add_q7.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_depthwise_conv_nt_t_padded_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_depthwise_conv_nt_t_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_mat_mul_core_1x_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_mat_mul_core_4x_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_mat_mul_kernel_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_mat_mult_nt_t_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_mult_q15.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_mult_q7.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_vec_mat_mult_t_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_vec_mat_mult_t_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nn_vec_mat_mult_t_svdf_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_nntables.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_q7_to_q15_no_shift.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_q7_to_q15_reordered_no_shift.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_q7_to_q15_reordered_with_offset.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/NNSupportFunctions/arm_q7_to_q15_with_offset.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_mat_q7_vec_q15.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_mat_q7_vec_q15_opt.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_q15.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_q15_opt.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_q7.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_q7_opt.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_1_x_n_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_1x1_HWC_q7_fast_nonsquare.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_1x1_s8_fast.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q15_basic.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q15_fast.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q15_fast_nonsquare.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q7_RGB.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q7_basic.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q7_basic_nonsquare.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q7_fast.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q7_fast_nonsquare.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_fast_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_wrapper_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_wrapper_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_3x3_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_s8_opt.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_u8_basic_ver1.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_wrapper_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_separable_conv_HWC_q7.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_separable_conv_HWC_q7_nonsquare.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_nn_depthwise_conv_s8_core.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_nn_mat_mult_kernel_q7_q15.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_nn_mat_mult_kernel_q7_q15_reordered.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_nn_mat_mult_kernel_s8_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConvolutionFunctions/arm_nn_mat_mult_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConcatenationFunctions/arm_concatenation_s8_w.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConcatenationFunctions/arm_concatenation_s8_x.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConcatenationFunctions/arm_concatenation_s8_y.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ConcatenationFunctions/arm_concatenation_s8_z.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/BasicMathFunctions/arm_elementwise_add_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/BasicMathFunctions/arm_elementwise_add_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/BasicMathFunctions/arm_elementwise_mul_s16.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/BasicMathFunctions/arm_elementwise_mul_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ActivationFunctions/arm_nn_activations_q15.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ActivationFunctions/arm_nn_activations_q7.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ActivationFunctions/arm_relu6_s8.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ActivationFunctions/arm_relu_q15.o ./eiq/tensorflow-lite/third_party/cmsis/CMSIS/NN/Source/ActivationFunctions/arm_relu_q7.o ./eiq/tensorflow-lite/tensorflow/lite/schema/schema_utils.o ./eiq/tensorflow-lite/tensorflow/lite/micro/memory_planner/greedy_memory_planner.o ./eiq/tensorflow-lite/tensorflow/lite/micro/memory_planner/linear_memory_planner.o ./eiq/tensorflow-lite/tensorflow/lite/micro/memory_planner/non_persistent_buffer_planner_shim.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/cmsis_nn/add.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/cmsis_nn/conv.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/cmsis_nn/depthwise_conv.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/cmsis_nn/fully_connected.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/cmsis_nn/mul.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/cmsis_nn/pooling.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/cmsis_nn/softmax.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/cmsis_nn/svdf.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/activations.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/activations_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/add.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/add_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/add_n.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/arg_min_max.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/assign_variable.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/batch_to_space_nd.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/broadcast_args.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/broadcast_to.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/call_once.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/cast.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/ceil.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/circular_buffer.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/circular_buffer_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/comparisons.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/concatenation.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/conv.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/conv_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/cumsum.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/depth_to_space.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/depthwise_conv.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/depthwise_conv_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/dequantize.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/dequantize_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/detection_postprocess.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/div.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/elementwise.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/elu.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/ethosu.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/exp.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/expand_dims.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/fill.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/floor.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/floor_div.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/floor_mod.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/fully_connected.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/fully_connected_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/gather.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/gather_nd.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/hard_swish.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/hard_swish_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/if.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/kernel_util.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/l2_pool_2d.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/l2norm.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/leaky_relu.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/leaky_relu_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/log_softmax.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/logical.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/logical_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/logistic.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/logistic_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/lstm_eval.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/maximum_minimum.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/micro_tensor_utils.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/mirror_pad.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/mul.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/mul_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/neg.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/pack.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/pad.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/pooling.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/pooling_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/prelu.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/prelu_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/quantize.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/quantize_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/read_variable.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/reduce.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/reduce_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/reshape.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/resize_bilinear.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/resize_nearest_neighbor.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/round.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/select.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/shape.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/slice.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/softmax.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/softmax_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/space_to_batch_nd.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/space_to_depth.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/split.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/split_v.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/squared_difference.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/squeeze.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/strided_slice.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/sub.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/sub_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/svdf.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/svdf_common.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/tanh.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/transpose.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/transpose_conv.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/unidirectional_sequence_lstm.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/unpack.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/var_handle.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/while.o ./eiq/tensorflow-lite/tensorflow/lite/micro/kernels/zeros_like.o ./eiq/tensorflow-lite/tensorflow/lite/micro/arena_allocator/non_persistent_arena_buffer_allocator.o ./eiq/tensorflow-lite/tensorflow/lite/micro/arena_allocator/persistent_arena_buffer_allocator.o ./eiq/tensorflow-lite/tensorflow/lite/micro/arena_allocator/recording_single_arena_buffer_allocator.o ./eiq/tensorflow-lite/tensorflow/lite/micro/arena_allocator/single_arena_buffer_allocator.o ./eiq/tensorflow-lite/tensorflow/lite/micro/all_ops_resolver.o ./eiq/tensorflow-lite/tensorflow/lite/micro/debug_log.o ./eiq/tensorflow-lite/tensorflow/lite/micro/fake_micro_context.o ./eiq/tensorflow-lite/tensorflow/lite/micro/flatbuffer_utils.o ./eiq/tensorflow-lite/tensorflow/lite/micro/memory_helpers.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_allocation_info.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_allocator.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_context.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_error_reporter.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_graph.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_interpreter.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_log.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_profiler.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_resource_variable.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_string.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_time.o ./eiq/tensorflow-lite/tensorflow/lite/micro/micro_utils.o ./eiq/tensorflow-lite/tensorflow/lite/micro/recording_micro_allocator.o ./eiq/tensorflow-lite/tensorflow/lite/kernels/internal/reference/portable_tensor_utils.o ./eiq/tensorflow-lite/tensorflow/lite/kernels/internal/quantization_util.o ./eiq/tensorflow-lite/tensorflow/lite/kernels/kernel_utils.o ./eiq/tensorflow-lite/tensorflow/lite/core/api/error_reporter.o ./eiq/tensorflow-lite/tensorflow/lite/core/api/flatbuffer_conversions.o ./eiq/tensorflow-lite/tensorflow/lite/core/api/op_resolver.o ./eiq/tensorflow-lite/tensorflow/lite/core/api/tensor_utils.o ./eiq/tensorflow-lite/tensorflow/lite/c/common.o ./drivers/fsl_clock.o ./drivers/fsl_common.o ./drivers/fsl_common_arm.o ./drivers/fsl_flexcomm.o ./drivers/fsl_gpio.o ./drivers/fsl_i2c.o ./drivers/fsl_power.o ./drivers/fsl_reset.o ./drivers/fsl_usart.o ./device/system_LPC55S69_cm33_core0.o ./component/uart/fsl_adapter_usart.o ./component/serial_manager/fsl_component_serial_manager.o ./component/serial_manager/fsl_component_serial_port_uart.o ./component/lists/fsl_component_generic_list.o ./board/board.o ./board/board_init.o ./board/clock_config.o ./board/peripherals.o ./board/pin_mux.o ./CMSIS/DSP/Source/TransformFunctions/TransformFunctions.o ./CMSIS/DSP/Source/TransformFunctions/TransformFunctionsF16.o ./CMSIS/DSP/Source/TransformFunctions/arm_bitreversal.o ./CMSIS/DSP/Source/TransformFunctions/arm_bitreversal2.o ./CMSIS/DSP/Source/TransformFunctions/arm_bitreversal_f16.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_f16.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_f64.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_init_f16.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_init_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_init_f64.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_init_q15.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_init_q31.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_q15.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_q31.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix2_f16.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix2_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix2_init_f16.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix2_init_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix2_init_q15.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix2_init_q31.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix2_q15.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix2_q31.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix4_f16.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix4_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix4_init_f16.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix4_init_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix4_init_q15.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix4_init_q31.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix4_q15.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix4_q31.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix8_f16.o ./CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix8_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_dct4_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_dct4_init_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_dct4_init_q15.o ./CMSIS/DSP/Source/TransformFunctions/arm_dct4_init_q31.o ./CMSIS/DSP/Source/TransformFunctions/arm_dct4_q15.o ./CMSIS/DSP/Source/TransformFunctions/arm_dct4_q31.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_fast_f16.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_fast_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_fast_f64.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_fast_init_f16.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_fast_init_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_fast_init_f64.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_init_f32.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_init_q15.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_init_q31.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_q15.o ./CMSIS/DSP/Source/TransformFunctions/arm_rfft_q31.o ./CMSIS/DSP/Source/SupportFunctions/SupportFunctions.o ./CMSIS/DSP/Source/SupportFunctions/SupportFunctionsF16.o ./CMSIS/DSP/Source/SupportFunctions/arm_barycenter_f16.o ./CMSIS/DSP/Source/SupportFunctions/arm_barycenter_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_bitonic_sort_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_bubble_sort_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_copy_f16.o ./CMSIS/DSP/Source/SupportFunctions/arm_copy_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_copy_q15.o ./CMSIS/DSP/Source/SupportFunctions/arm_copy_q31.o ./CMSIS/DSP/Source/SupportFunctions/arm_copy_q7.o ./CMSIS/DSP/Source/SupportFunctions/arm_f16_to_float.o ./CMSIS/DSP/Source/SupportFunctions/arm_f16_to_q15.o ./CMSIS/DSP/Source/SupportFunctions/arm_fill_f16.o ./CMSIS/DSP/Source/SupportFunctions/arm_fill_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_fill_q15.o ./CMSIS/DSP/Source/SupportFunctions/arm_fill_q31.o ./CMSIS/DSP/Source/SupportFunctions/arm_fill_q7.o ./CMSIS/DSP/Source/SupportFunctions/arm_float_to_f16.o ./CMSIS/DSP/Source/SupportFunctions/arm_float_to_q15.o ./CMSIS/DSP/Source/SupportFunctions/arm_float_to_q31.o ./CMSIS/DSP/Source/SupportFunctions/arm_float_to_q7.o ./CMSIS/DSP/Source/SupportFunctions/arm_heap_sort_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_insertion_sort_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_merge_sort_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_merge_sort_init_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_q15_to_f16.o ./CMSIS/DSP/Source/SupportFunctions/arm_q15_to_float.o ./CMSIS/DSP/Source/SupportFunctions/arm_q15_to_q31.o ./CMSIS/DSP/Source/SupportFunctions/arm_q15_to_q7.o ./CMSIS/DSP/Source/SupportFunctions/arm_q31_to_float.o ./CMSIS/DSP/Source/SupportFunctions/arm_q31_to_q15.o ./CMSIS/DSP/Source/SupportFunctions/arm_q31_to_q7.o ./CMSIS/DSP/Source/SupportFunctions/arm_q7_to_float.o ./CMSIS/DSP/Source/SupportFunctions/arm_q7_to_q15.o ./CMSIS/DSP/Source/SupportFunctions/arm_q7_to_q31.o ./CMSIS/DSP/Source/SupportFunctions/arm_quick_sort_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_selection_sort_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_sort_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_sort_init_f32.o ./CMSIS/DSP/Source/SupportFunctions/arm_weighted_sum_f16.o ./CMSIS/DSP/Source/SupportFunctions/arm_weighted_sum_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/StatisticsFunctions.o ./CMSIS/DSP/Source/StatisticsFunctions/StatisticsFunctionsF16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_absmax_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_absmax_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_absmax_q15.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_absmax_q31.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_absmax_q7.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_absmin_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_absmin_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_absmin_q15.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_absmin_q31.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_absmin_q7.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_entropy_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_entropy_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_entropy_f64.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_kullback_leibler_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_kullback_leibler_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_kullback_leibler_f64.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_logsumexp_dot_prod_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_logsumexp_dot_prod_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_logsumexp_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_logsumexp_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_max_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_max_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_max_no_idx_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_max_no_idx_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_max_q15.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_max_q31.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_max_q7.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_mean_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_mean_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_mean_q15.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_mean_q31.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_mean_q7.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_min_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_min_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_min_q15.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_min_q31.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_min_q7.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_power_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_power_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_power_q15.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_power_q31.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_power_q7.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_rms_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_rms_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_rms_q15.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_rms_q31.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_std_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_std_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_std_q15.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_std_q31.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_var_f16.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_var_f32.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_var_q15.o ./CMSIS/DSP/Source/StatisticsFunctions/arm_var_q31.o ./CMSIS/DSP/Source/SVMFunctions/SVMFunctions.o ./CMSIS/DSP/Source/SVMFunctions/SVMFunctionsF16.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_linear_init_f16.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_linear_init_f32.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_linear_predict_f16.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_linear_predict_f32.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_polynomial_init_f16.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_polynomial_init_f32.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_polynomial_predict_f16.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_polynomial_predict_f32.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_rbf_init_f16.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_rbf_init_f32.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_rbf_predict_f16.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_rbf_predict_f32.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_sigmoid_init_f16.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_sigmoid_init_f32.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_sigmoid_predict_f16.o ./CMSIS/DSP/Source/SVMFunctions/arm_svm_sigmoid_predict_f32.o ./CMSIS/DSP/Source/QuaternionMathFunctions/QuaternionMathFunctions.o ./CMSIS/DSP/Source/QuaternionMathFunctions/arm_quaternion2rotation_f32.o ./CMSIS/DSP/Source/QuaternionMathFunctions/arm_quaternion_conjugate_f32.o ./CMSIS/DSP/Source/QuaternionMathFunctions/arm_quaternion_inverse_f32.o ./CMSIS/DSP/Source/QuaternionMathFunctions/arm_quaternion_norm_f32.o ./CMSIS/DSP/Source/QuaternionMathFunctions/arm_quaternion_normalize_f32.o ./CMSIS/DSP/Source/QuaternionMathFunctions/arm_quaternion_product_f32.o ./CMSIS/DSP/Source/QuaternionMathFunctions/arm_quaternion_product_single_f32.o ./CMSIS/DSP/Source/QuaternionMathFunctions/arm_rotation2quaternion_f32.o ./CMSIS/DSP/Source/MatrixFunctions/MatrixFunctions.o ./CMSIS/DSP/Source/MatrixFunctions/MatrixFunctionsF16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_add_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_add_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_add_q15.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_add_q31.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cholesky_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cholesky_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cholesky_f64.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cmplx_mult_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cmplx_mult_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cmplx_mult_q15.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cmplx_mult_q31.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cmplx_trans_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cmplx_trans_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cmplx_trans_q15.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_cmplx_trans_q31.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_init_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_init_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_init_q15.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_init_q31.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_inverse_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_inverse_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_inverse_f64.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_ldlt_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_ldlt_f64.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_mult_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_mult_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_mult_f64.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_mult_fast_q15.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_mult_fast_q31.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_mult_q15.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_mult_q31.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_mult_q7.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_scale_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_scale_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_scale_q15.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_scale_q31.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_solve_lower_triangular_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_solve_lower_triangular_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_solve_lower_triangular_f64.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_solve_upper_triangular_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_solve_upper_triangular_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_solve_upper_triangular_f64.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_sub_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_sub_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_sub_f64.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_sub_q15.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_sub_q31.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_trans_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_trans_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_trans_f64.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_trans_q15.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_trans_q31.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_trans_q7.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_vec_mult_f16.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_vec_mult_f32.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_vec_mult_q15.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_vec_mult_q31.o ./CMSIS/DSP/Source/MatrixFunctions/arm_mat_vec_mult_q7.o ./CMSIS/DSP/Source/InterpolationFunctions/InterpolationFunctions.o ./CMSIS/DSP/Source/InterpolationFunctions/InterpolationFunctionsF16.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_bilinear_interp_f16.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_bilinear_interp_f32.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_bilinear_interp_q15.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_bilinear_interp_q31.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_bilinear_interp_q7.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_linear_interp_f16.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_linear_interp_f32.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_linear_interp_q15.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_linear_interp_q31.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_linear_interp_q7.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_spline_interp_f32.o ./CMSIS/DSP/Source/InterpolationFunctions/arm_spline_interp_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/FilteringFunctions.o ./CMSIS/DSP/Source/FilteringFunctions/FilteringFunctionsF16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_32x64_init_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_32x64_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_f16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_fast_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_fast_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_init_f16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_init_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_init_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df1_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df2T_f16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df2T_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df2T_f64.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df2T_init_f16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df2T_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_df2T_init_f64.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_stereo_df2T_f16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_stereo_df2T_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_stereo_df2T_init_f16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_biquad_cascade_stereo_df2T_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_fast_opt_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_fast_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_fast_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_opt_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_opt_q7.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_partial_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_partial_fast_opt_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_partial_fast_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_partial_fast_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_partial_opt_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_partial_opt_q7.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_partial_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_partial_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_partial_q7.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_conv_q7.o ./CMSIS/DSP/Source/FilteringFunctions/arm_correlate_f16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_correlate_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_correlate_fast_opt_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_correlate_fast_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_correlate_fast_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_correlate_opt_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_correlate_opt_q7.o ./CMSIS/DSP/Source/FilteringFunctions/arm_correlate_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_correlate_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_correlate_q7.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_decimate_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_decimate_fast_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_decimate_fast_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_decimate_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_decimate_init_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_decimate_init_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_decimate_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_decimate_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_f16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_fast_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_fast_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_init_f16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_init_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_init_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_init_q7.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_interpolate_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_interpolate_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_interpolate_init_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_interpolate_init_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_interpolate_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_interpolate_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_lattice_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_lattice_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_lattice_init_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_lattice_init_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_lattice_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_lattice_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_q7.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_sparse_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_sparse_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_sparse_init_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_sparse_init_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_sparse_init_q7.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_sparse_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_sparse_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_fir_sparse_q7.o ./CMSIS/DSP/Source/FilteringFunctions/arm_iir_lattice_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_iir_lattice_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_iir_lattice_init_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_iir_lattice_init_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_iir_lattice_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_iir_lattice_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_levinson_durbin_f16.o ./CMSIS/DSP/Source/FilteringFunctions/arm_levinson_durbin_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_levinson_durbin_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_init_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_init_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_norm_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_norm_init_f32.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_norm_init_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_norm_init_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_norm_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_norm_q31.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_q15.o ./CMSIS/DSP/Source/FilteringFunctions/arm_lms_q31.o ./CMSIS/DSP/Source/FastMathFunctions/FastMathFunctions.o ./CMSIS/DSP/Source/FastMathFunctions/FastMathFunctionsF16.o ./CMSIS/DSP/Source/FastMathFunctions/arm_cos_f32.o ./CMSIS/DSP/Source/FastMathFunctions/arm_cos_q15.o ./CMSIS/DSP/Source/FastMathFunctions/arm_cos_q31.o ./CMSIS/DSP/Source/FastMathFunctions/arm_divide_q15.o ./CMSIS/DSP/Source/FastMathFunctions/arm_sin_f32.o ./CMSIS/DSP/Source/FastMathFunctions/arm_sin_q15.o ./CMSIS/DSP/Source/FastMathFunctions/arm_sin_q31.o ./CMSIS/DSP/Source/FastMathFunctions/arm_sqrt_q15.o ./CMSIS/DSP/Source/FastMathFunctions/arm_sqrt_q31.o ./CMSIS/DSP/Source/FastMathFunctions/arm_vexp_f16.o ./CMSIS/DSP/Source/FastMathFunctions/arm_vexp_f32.o ./CMSIS/DSP/Source/FastMathFunctions/arm_vinverse_f16.o ./CMSIS/DSP/Source/FastMathFunctions/arm_vlog_f16.o ./CMSIS/DSP/Source/FastMathFunctions/arm_vlog_f32.o ./CMSIS/DSP/Source/DistanceFunctions/DistanceFunctions.o ./CMSIS/DSP/Source/DistanceFunctions/DistanceFunctionsF16.o ./CMSIS/DSP/Source/DistanceFunctions/arm_boolean_distance.o ./CMSIS/DSP/Source/DistanceFunctions/arm_braycurtis_distance_f16.o ./CMSIS/DSP/Source/DistanceFunctions/arm_braycurtis_distance_f32.o ./CMSIS/DSP/Source/DistanceFunctions/arm_canberra_distance_f16.o ./CMSIS/DSP/Source/DistanceFunctions/arm_canberra_distance_f32.o ./CMSIS/DSP/Source/DistanceFunctions/arm_chebyshev_distance_f16.o ./CMSIS/DSP/Source/DistanceFunctions/arm_chebyshev_distance_f32.o ./CMSIS/DSP/Source/DistanceFunctions/arm_cityblock_distance_f16.o ./CMSIS/DSP/Source/DistanceFunctions/arm_cityblock_distance_f32.o ./CMSIS/DSP/Source/DistanceFunctions/arm_correlation_distance_f16.o ./CMSIS/DSP/Source/DistanceFunctions/arm_correlation_distance_f32.o ./CMSIS/DSP/Source/DistanceFunctions/arm_cosine_distance_f16.o ./CMSIS/DSP/Source/DistanceFunctions/arm_cosine_distance_f32.o ./CMSIS/DSP/Source/DistanceFunctions/arm_dice_distance.o ./CMSIS/DSP/Source/DistanceFunctions/arm_euclidean_distance_f16.o ./CMSIS/DSP/Source/DistanceFunctions/arm_euclidean_distance_f32.o ./CMSIS/DSP/Source/DistanceFunctions/arm_hamming_distance.o ./CMSIS/DSP/Source/DistanceFunctions/arm_jaccard_distance.o ./CMSIS/DSP/Source/DistanceFunctions/arm_jensenshannon_distance_f16.o ./CMSIS/DSP/Source/DistanceFunctions/arm_jensenshannon_distance_f32.o ./CMSIS/DSP/Source/DistanceFunctions/arm_kulsinski_distance.o ./CMSIS/DSP/Source/DistanceFunctions/arm_minkowski_distance_f16.o ./CMSIS/DSP/Source/DistanceFunctions/arm_minkowski_distance_f32.o ./CMSIS/DSP/Source/DistanceFunctions/arm_rogerstanimoto_distance.o ./CMSIS/DSP/Source/DistanceFunctions/arm_russellrao_distance.o ./CMSIS/DSP/Source/DistanceFunctions/arm_sokalmichener_distance.o ./CMSIS/DSP/Source/DistanceFunctions/arm_sokalsneath_distance.o ./CMSIS/DSP/Source/DistanceFunctions/arm_yule_distance.o ./CMSIS/DSP/Source/ControllerFunctions/ControllerFunctions.o ./CMSIS/DSP/Source/ControllerFunctions/arm_pid_init_f32.o ./CMSIS/DSP/Source/ControllerFunctions/arm_pid_init_q15.o ./CMSIS/DSP/Source/ControllerFunctions/arm_pid_init_q31.o ./CMSIS/DSP/Source/ControllerFunctions/arm_pid_reset_f32.o ./CMSIS/DSP/Source/ControllerFunctions/arm_pid_reset_q15.o ./CMSIS/DSP/Source/ControllerFunctions/arm_pid_reset_q31.o ./CMSIS/DSP/Source/ControllerFunctions/arm_sin_cos_f32.o ./CMSIS/DSP/Source/ControllerFunctions/arm_sin_cos_q31.o ./CMSIS/DSP/Source/ComplexMathFunctions/ComplexMathFunctions.o ./CMSIS/DSP/Source/ComplexMathFunctions/ComplexMathFunctionsF16.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_conj_f16.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_conj_f32.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_conj_q15.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_conj_q31.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_dot_prod_f16.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_dot_prod_f32.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_dot_prod_q15.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_dot_prod_q31.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mag_f16.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mag_f32.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mag_q15.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mag_q31.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mag_squared_f16.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mag_squared_f32.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mag_squared_q15.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mag_squared_q31.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mult_cmplx_f16.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mult_cmplx_f32.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mult_cmplx_q15.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mult_cmplx_q31.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mult_real_f16.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mult_real_f32.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mult_real_q15.o ./CMSIS/DSP/Source/ComplexMathFunctions/arm_cmplx_mult_real_q31.o ./CMSIS/DSP/Source/CommonTables/CommonTables.o ./CMSIS/DSP/Source/CommonTables/CommonTablesF16.o ./CMSIS/DSP/Source/CommonTables/arm_common_tables.o ./CMSIS/DSP/Source/CommonTables/arm_common_tables_f16.o ./CMSIS/DSP/Source/CommonTables/arm_const_structs.o ./CMSIS/DSP/Source/CommonTables/arm_const_structs_f16.o ./CMSIS/DSP/Source/CommonTables/arm_mve_tables.o ./CMSIS/DSP/Source/CommonTables/arm_mve_tables_f16.o ./CMSIS/DSP/Source/BayesFunctions/BayesFunctions.o ./CMSIS/DSP/Source/BayesFunctions/BayesFunctionsF16.o ./CMSIS/DSP/Source/BayesFunctions/arm_gaussian_naive_bayes_predict_f16.o ./CMSIS/DSP/Source/BayesFunctions/arm_gaussian_naive_bayes_predict_f32.o ./CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctions.o ./CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctionsF16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_abs_f16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_abs_f32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_abs_q15.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_abs_q31.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_abs_q7.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_add_f16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_add_f32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_add_q15.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_add_q31.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_add_q7.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_and_u16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_and_u32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_and_u8.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_clip_f16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_clip_f32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_clip_q15.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_clip_q31.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_clip_q7.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_dot_prod_f16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_dot_prod_f32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_dot_prod_q15.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_dot_prod_q31.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_dot_prod_q7.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_mult_f16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_mult_f32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_mult_q15.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_mult_q31.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_mult_q7.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_negate_f16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_negate_f32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_negate_q15.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_negate_q31.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_negate_q7.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_not_u16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_not_u32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_not_u8.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_offset_f16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_offset_f32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_offset_q15.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_offset_q31.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_offset_q7.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_or_u16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_or_u32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_or_u8.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_scale_f16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_scale_f32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_scale_q15.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_scale_q31.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_scale_q7.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_shift_q15.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_shift_q31.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_shift_q7.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_sub_f16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_sub_f32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_sub_q15.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_sub_q31.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_sub_q7.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_xor_u16.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_xor_u32.o ./CMSIS/DSP/Source/BasicMathFunctions/arm_xor_u8.o
process_begin: CreateProcess(...) failed.
make (e=87): The parameter is incorrect.

make[1]: *** [makefile:105: evklpc55S69_tflm_kws_eiq.axf] Error 87
make: *** [makefile:96: all] Error 2
"make -r -j8 all" terminated with exit code 2. Build might be incomplete. 2

Where should I look specifically? This project was done for LPC55S89
I build the same project on MIMXRT1064 and I did not get any error(I attached that result as new2.txt)
Note: I deleted what was included in CreateProcess to not pass message limit(in the attached document, it has full version)

0 Kudos
Reply
2 Replies

7,022 Views
lpcxpresso_supp
NXP Employee
NXP Employee

As far as I can tell, the command line for the linker is ~50k in your case, meaning that is above the 32k limit allowed by Windows API (CreateProcess).

There's also a long-standing Eclipse bug (see [1]) on this topic. Unfortunately, there's no indication that the proposed fix will eventually reach the mainline.

Given the huge list of objects passed to the linker, I suggest you split your app in logical components / libraries, thus workaround the issue you encountered.

Regards,
MCUXpresso IDE Support

[1] https://bugs.eclipse.org/bugs/show_bug.cgi?id=72965

0 Kudos
Reply

7,016 Views
Emin
Contributor III

It is indeed above 32K limit. I checked with the other project I did on MIMXRT1064, where some files are not actually included in compile list. By excluding them I was able to fully compile the project I made on LPC55S69

0 Kudos
Reply