how to define a project name when I import a SDK example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to define a project name when I import a SDK example

1,579 Views
neoxiong
NXP Employee
NXP Employee

There is only prefix and postfix I can set when importing a SDK example, can I set a full name?

The use case is my application is very close to one of SDK example but I need use, e.g, 'myproject' as name.

0 Kudos
Reply
2 Replies

1,483 Views
lpcxpresso_supp
NXP Employee
NXP Employee

There is no way to completely control the name of the generated project when you import a project, only to change the prefix or postfix string added to the example's name.

If you want to have a completely different name, then import the example, then right click on it in the Project Explorer view and select "Rename".

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

1,483 Views
neoxiong
NXP Employee
NXP Employee

Got it, thanks.

Since project cloner in the mcuxpresso tool can have a totally different name, and that tool does not support mucx, I would suggest we give this flexibility to user.

0 Kudos
Reply