foreard-looking Project setup in MCUExpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

foreard-looking Project setup in MCUExpresso

1,945 次查看
christianhonegg
Contributor I

We started our project based on a SDK example.

Now, how do we need to re-arrange our files in order to be able to update the SDK with minimal effort on our own files?

0 项奖励
回复
1 回复

1,756 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Christian.

I am not sure if I understand your question accurately. From I understanding you started your project based on an existing SDK demo code, and you need add your own code/file to it. Correct?

If yes, you can do it. But we need to know SDK uses its own header file, start up code,etc. User code must  be compatible with these SDK files. Thus I suggest you add user code part by part. If you need add new file, please also make sure the file path is included in the project path setting.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复