debug Err LCP1769 DAP board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

debug Err LCP1769 DAP board

2,351件の閲覧回数
nauman_1015
Contributor I

I was trying to debug LCP1769 DAP board with mcuexpresso IDE but it does not launch debug process. Instead i get this message below. Kindly help me to know what is the problem and how should i rectify it??

MCUXpresso IDE RedlinkMulti Driver v11.0 (Aug 27 2019 16:46:33 - crt_emu_cm_redlink build 22)
Found part description in XML file nxp_lpc17xx.xme
Reconnected to existing LinkServer process.
connection failed - Em(01). Cannot find MEM-AP selected by core index (check target power).. Retrying
Failed on connect: Em(01). Cannot find MEM-AP selected by core index (check target power)
Connected&Reset. Was: NotConnected. DpID: 2BA01477. CpuID: 00000000. Info: <None>
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 0
No debug bus (MemAp) selected
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
(100) Target Connection Failed

0 件の賞賛
返信
1 返信

2,321件の閲覧回数
converse
Senior Contributor V

The clue may be in the message - check target power.

make sure sufficient power is being supplied to your board.

0 件の賞賛
返信