cJSON - undefined reference to __isnan

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cJSON - undefined reference to __isnan

Jump to solution
6,733 Views
nickwallis
Senior Contributor I

Hi,

I am using cJSON is a project but am having an issue building it that I don't understand.

If I include references to cJSON_Print(), then the build fails with an error message "undefined reference to __isnan". This is despite the fact that this is available to the build, in math.h (which is #included).

Why would the build fail in this way, even though the required definition/file is actually there?

thanks

-Nick

 

0 Kudos
Reply
1 Solution
6,673 Views
nickwallis
Senior Contributor I

I got some time to look into this, and on second glance it seemed obvious that Redlib was missing these dependencies, and changing to Newlib has fixed this. Thanks.

View solution in original post

0 Kudos
Reply
4 Replies
6,674 Views
nickwallis
Senior Contributor I

I got some time to look into this, and on second glance it seemed obvious that Redlib was missing these dependencies, and changing to Newlib has fixed this. Thanks.

0 Kudos
Reply
6,726 Views
converse
Senior Contributor V

The error is for __isnand not isnan...

0 Kudos
Reply
6,722 Views
nickwallis
Senior Contributor I

Exactly my point. The error message does not match the code.

Here is the code:

/* Render the number nicely from the given item into a string. */
static cJSON_bool print_number(const cJSON * const item, printbuffer * const output_buffer)
{
    unsigned char *output_pointer = NULL;
    double d = item->valuedouble;
    int length = 0;
    size_t i = 0;
    unsigned char number_buffer[26] = {0}; /* temporary buffer to print the number into */
    unsigned char decimal_point = get_decimal_point();
    double test = 0.0;

    if (output_buffer == NULL)
    {
        return false;
    }

    /* This checks for NaN and Infinity */

    if (isnan(d) || isinf(d))
    {
        length = sprintf((char*)number_buffer, "null");
    }
    else
    { ..........

And here is the compiler error:

C:\mcuxpresso_workspace\sdm_01\Debug/../source/cJSON.c:562: undefined reference to `__isnand'

If I CTRL-click on the isnan in the code, then it takes me to the definition in math.h as expected.

So, why the compiler error? The code looks OK to me.

Thanks,

-Nick

0 Kudos
Reply
6,718 Views
converse
Senior Contributor V

Just to clarify. It is a linker error not a compiler error. That is, you are missing a library. You need to provide a library to satisfy the isnand function 

0 Kudos
Reply