Where does MCUX IDE get its default J-Link path from?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where does MCUX IDE get its default J-Link path from?

1,912件の閲覧回数
dmarks_ls
Senior Contributor II

Today I cleaned out all my old SEGGER J-Link software installations, then installed the latest (v8.12e) into C:\Program Files\SEGGER\JLink ("update existing installation").  I just went to debug one of my programs, and the IDE is complaining that J-Link support is unavailable (while conveniently not mentioning where it's looking).

jlink_unavailable.png

If I click Yes, I'm given a file dialog to select the J-Link folder, which gets filled into the J-Link options (see below).  Alternately, if I go into Window / Preferences, search "J", and select J-Link Options, I can see the options dialog where at the top is listed what MCUX thinks is my default J-Link directory:

jlink_options.png

I did have J-Link installed to that path, but I removed it.  And I now have "C:\Program Files\SEGGER\JLink" in the "Custom path" and everything works fine.

My question is... where does MCUX IDE get the "Default path" from?  It's not an environment variable, I checked.  Is it set when a given version of MCUX is installed, and you can't change it again for this installation?  As I said, I've set a custom path to get myself working, but I'm just curious how MCUX picks the default path.

Dana M.

0 件の賞賛
返信
1 返信

1,895件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @dmarks_ls ,

Thanks for your post. You can refer to the "MCUXpresso IDE xx.x User Guide". Taking MCUXpresso 24.9 as an example, the path is C:\NXP\MCUXpressoIDE_24.9.25.

Celeste_Liu_0-1739328705619.png

In the "13.9.1 SEGGER software installation" section, it provides a detailed description of how the IDE locates a SEGGER installation.

Celeste_Liu_1-1739328878629.png

Hope it can help you.  Any new issues, welcome to create the new post.

Have a good day,

Celeste

 

----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信