Target reported errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Target reported errors

3,588 Views
Prudhvi_Raj
Contributor I

Tried to debug sdk by MCUXpresso IDE ,occuring a error such as target reported errors .provide solution as soon as possible.

Refer to the attachment.

0 Kudos
Reply
4 Replies

3,559 Views
Prudhvi_Raj
Contributor I

Hi @Harry_Zhang 

The board is powered by debug port and tried to debug, still i am getting the same error same as earlier.

0 Kudos
Reply

3,546 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Prudhvi_Raj 

On another board, i reproduced this issue.

HangZhang_1-1718272093484.png

When i changed to jlink.

It can work.

HangZhang_2-1718272156104.png

Hope this will help you.

BR

Hang

0 Kudos
Reply

3,549 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Prudhvi_Raj 

I tested my board, 

HangZhang_0-1718266886254.png

HangZhang_1-1718266954292.png

It can work.

I watched your error message,

It reported that the wire not connected,

So can you change another wire?

BR

Hang

 

0 Kudos
Reply

3,570 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Prudhvi_Raj 

According to the picture, this error is due to not connecting to the core.

So please check if this board is powered on and if it is connected to the debug port.

Hope this will help you.

BR

Hang

0 Kudos
Reply