TWR-KV46F150M Debugging Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-KV46F150M Debugging Support

1,760 Views
deepak_keswani
Contributor I

Hi,

I am using TWR-KV46F150M Tower Module Board. I have imported MCUXpresso SDK examples to the IDE. Now when I am trying to flash the examples to the tower module, I am not able to do. On checking debugger options in Debug Configurations(Image is Attached), I am not able to see Port number getting reflected in it.Although, in Device Manager port number (COM6) is coming for the debugger.

Also, In supported boards under MCUXpresso IDE section, i am not able to find KV4x series micro-controller in it. So can anybody help me in resolving the above problem?

Thanks

Regards

Deepak Keswani

0 Kudos
Reply
1 Reply

1,637 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Deepak Keswani,

Please use the debug button in "Quickstart Panel" :

pastedImage_1.png

Also please check jumpers on board refer to "Default Jumpers" of User Guide:

https://www.nxp.com/docs/en/user-guide/TWRKV46F150MUG.pdf    


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply