Starting debugger using MCUXpresso fails under Debian

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Starting debugger using MCUXpresso fails under Debian

1,381 次查看
achampoux
Contributor I

IDE: MCUXpresso v11.8.0

SDK: SDK_2_14_0_MIMXRT1170-EVKB-LINUX

Target board: MIMXRT1170-EVKB

Trying debug an m7 project fails with the message: 'Launching m7 LinkServer Debug' has encountered a problem, problem file does not exist. The file path to the binary is "m7/Debug\m7.axf", which contains an error as it contains a "\" instead of "/". The build is successful, the board is detected and the file does "m7/debug/m7.axf" exists.

Any way to fix this? 

Thanks.

0 项奖励
回复
1 回复

1,326 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @achampoux 

How about first debug a SDK demo without any change?

 

BR

Alice

0 项奖励
回复