MCUXpresso ide command line tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso ide command line tools

2,033 Views
n_jacobs
Contributor I

Hello,

I would like to use the command line tools to setup a automated Jenkins build.

I used the MCUXpresso IDE Command Line User Guide Rev. 11.8.0 and tried for 2 day's to get a test build of the lpcopen examples in lpcopen_3_02_lpcxpresso_xpresso4337.zip to compile but could not get it working.

The command line user guide uses -application com.nxp.mcuxpresso.headless.application .

Searching the web i found some older threads where they used -application org.eclipse.cdt.managedbuilder.core.headlessbuild and i have got that working.

I succesfully used:

/usr/local/mcuxpressoide-11.8.0_1165/ide/mcuxpressoide -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data /home/testbox/lpcopen/lpcopen_3_02_lpcxpresso_xpresso4337 -importAll /home/testbox/lpcopen/lpcopen_3_02_lpcxpresso_xpresso4337 -cleanBuild all

Could you give me a working command example with  -application com.nxp.mcuxpresso.headless.application according the  MCUXpresso IDE Command Line User Guide Rev. 11.8.0  that does the same?

0 Kudos
Reply
2 Replies

1,998 Views
n_jacobs
Contributor I

Hello @Alice_Yang ,

I am afraid you don't really know your own product.

MCUXpresso is the enhanced successor of LPCXpresso and inherits almost all of the features of LPCXpresso.

See for instance: https://community.nxp.com/t5/LPCXpresso-IDE/Difference-between-MCUXpresso-LPCXpresso-and-their-free-...

LPCOpen is designed for LPCXpresso by NXP and the LPC processor line support including LPC4337 is integrated in MCUXpresso.

I already found the command -application org.eclipse.cdt.managedbuilder.core.headless in the 6,5 years old thread you also mention, but

i don't find anything about in in the MCUXpresso IDE Command Line User Guide Rev. 11.8.0.

If that is the preferred function to use on some processors or projects, i would expect it to be mentioned and preferably had the difference explained.

Is the function -application com.nxp.mcuxpresso.headless.application only for processors with external SDK or makefile projects?

Regards

Nico

0 Kudos
Reply

2,004 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @n_jacobs 

I think maybe  because "lpcopen_3_02_lpcxpresso_xpresso4337.zip " is not development by MCUXpresso IDE, while by eclipse, so can use command 

-application org.eclipse.cdt.managedbuilder.core.headless  

There is a blog from Eirch, also use the same command:

https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-li...  

 

BR

Alice

0 Kudos
Reply